Other Parts Discussed in Thread: OMAP3530, DM3730
Hi,
I use on a design an OMAP3530CBB with a PoP manufactured by micron based on 1bit/ECC nand flash (the same PoP populated on the beagle board).
Unfortunately, the micron POP is EOL and i need to migrate to a POP based on a 4bits ECC/512bytes Nand flash.
After reading the "Raw NAND ECC" wiki page and the micron application note (Enabling NAND On-Die ECC for OMAP3 Using Linux/Android OS with YAFFS2), i was wondering what will be the best solution.
Just for info, i don't plan to use the on-die ECC as it requires to cycle the NAND power supply.
My idea is to migrate from OMAP3530CBB to DM3730CBP and use a software solution.
Any suggestion will be greatly appreciated.
Regards
grp