Hi,
The DDR frequency of SDKV7.3 is 2133MHZ (4266 MTS). We want to increase it to 2347MHZ(2133*1.1).
So we use the Jacinto 7 DDRSS Register Configuration Tool and modify it to generate dtsi file.

/dts-v1/; #include "k3-j721e-som-p0.dtsi" //#include "k3-j721e-ddr-evm-lp4-4266.dtsi" #include "k3-j721e-ddr-evm-lp4-4694.dtsi" #include "k3-j721e-ddr.dtsi"
After recompiling uboot, enter Linux and execute the k3conf command and find the following log:
root@TDA4-Board:~# k3conf dump clocks 47 |--------------------------------------------------------------------------------| | VERSION INFO | |--------------------------------------------------------------------------------| | K3CONF | (version v0.1-45-g79f007c built Sat Apr 10 00:45:34 UTC 2021) | | SoC | J721E SR1.0 | | SYSFW | ABI: 3.1 (firmware version 0x0014 '20.8.5--v2020.08b (Terrific Lla)') | |--------------------------------------------------------------------------------| |---------------------------------------------------------------------------------------| | Device ID | Clock ID | Clock Name | Status | Clock Frequency | |---------------------------------------------------------------------------------------| | 47 | 0 | DEV_DDR0_DDRSS_VBUS_CLK | CLK_STATE_READY | 1000000000 | | 47 | 1 | DEV_DDR0_PLL_CTRL_CLK | CLK_STATE_READY | 500000000 | | 47 | 2 | DEV_DDR0_DDRSS_DDR_PLL_CLK | CLK_STATE_READY | 782336000 | | 47 | 3 | DEV_DDR0_DDRSS_CFG_CLK | CLK_STATE_READY | 125000000 | | 47 | 4 | DEV_DDR0_DDRSS_IO_CK_N | CLK_STATE_READY | 0 | | 47 | 5 | DEV_DDR0_DDRSS_IO_CK | CLK_STATE_READY | 0 | |---------------------------------------------------------------------------------------| root@TDA4-Board:~#
It seems that the frequency has not increased but decreased. DDR can reach 2166MHZ before changing the frequency.
I would like to ask what went wrong?
Thanks!