Part Number: TDA4VM
Hi , everyone:
I boot OS as EMMC mode, when I power on , it report "No FDT memory address configured" , and OS abort, it seem as memory device tree have not config yet, how can I modify it?
the log as below, please advise, thanks!
j7-evm login:
U-Boot SPL 2020.01-g2781231a33 (Apr 10 2021 - 01:08:23 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.1.1--v2021.01a (Terrific Lla')
Trying to boot from MMC1
Loading Environment from MMC... *** Warning - bad CRC, using default environment
init_env from device 17 not supported!
Starting ATF on ARM64 core...
NOTICE: BL31: v2.4(release):07.03.00.005-dirty
NOTICE: BL31: Built : 00:15:40, Apr 10 2021
U-Boot SPL 2020.01-g2781231a33 (Apr 10 2021 - 00:17:14 +0000)
SYSFW ABI: 3.1 (firmware rev 0x0015 '21.1.1--v2021.01a (Terrific Lla')
Detected: J7X-BASE-CPB rev E3
Detected: J7X-VSC8514-ETH rev E2
Trying to boot from MMC1
U-Boot 2020.01-g2781231a33 (Apr 10 2021 - 00:17:14 +0000)
SoC: J721E SR2.0
Model: Texas Instruments K3 J721E SoC
Board: J721EX-PM2-SOM rev E8
DRAM: 4 GiB
not found for dev hbmc-mux
Flash: 0 Bytes
MMC: sdhci@4f80000: 0, sdhci@4fb0000: 1
Loading Environment from MMC... OK
In: serial@2800000
Out: serial@2800000
Err: serial@2800000
Detected: J7X-BASE-CPB rev E3
Detected: J7X-VSC8514-ETH rev E2
Net: K3 CPSW: nuss_ver: 0x6BA00101 cpsw_ver: 0x6BA80100 ale_ver: 0x00293904 Ports:1 mdio_freq:1000000
Warning: ethernet@46000000 using MAC address from ROM
eth0: ethernet@46000000
Hit any key to stop autoboot: 0
mmc_init: -123, time 2001
SD/MMC found on device 1
mmc_init: -123, time 2001
mmc_init: -123, time 2001
mmc_init: -123, time 2001
mmc_init: -123, time 2001
mmc_init: -123, time 2001
libfdt fdt_check_header(): FDT_ERR_BADMAGIC
No FDT memory address configured. Please configure
the FDT address via "fdt addr <address>" command.
Aborting!
Bad Linux ARM64 Image magic!
=>