Part Number: TMS320VC5402
Hello!
since some months I am responsible for a very old project with a TMS320VC5402 DSP.
The old environment was CCS v2.21 under Windows98 until now.
We want to move to a newer environment - set up a new CCS project and port the old files from CCS v2.21 to v5.
Please correct me if I am wrong:
As far as I know, our DSP is supported up to CCS v5.5, which is only supported up to Windows 7, correct?
I found an installer for CCS v5.2 and installed it on a Windows7 laptop, and now I'm stuck because I don't have an available compiler for the C5402.
I have no idea where I can get a compiler.
Do you know if there is a download option/setting within the CCS itself to download the missing compiler?
Or can you give me a download link where the appropriate compilers are available?
Many thanks in advance.
Regards, Johanna