This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

set up dvsdk for omap3530

hello. I install DVSDK on host successfully with the instruction from . but I have a question about creating SD card. do I have to create SD card by following the step in the guide above? currently, I have installed open-embedded on the SD card. I wonder if code with dvsdk can run on the open-embedded . (I use codesourcery to do cross-compiling ) thanks ch