This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

66AK2G12: Yocto Project image rootfs password for 66ak2g12 image

Part Number: 66AK2G12

Hi,

 

 

I have used meta-ti layer (Version :Rocko ) to generate core-image-minimal for my 66ak2g12 board from TI. I’m able to boot up my board properly  but after booting up  not able to login.

I’ve tried “root” or blank password but still it’s throwing wrong password.

When I’m using “root” as a user then it throws “can’t set root user”.

 

In local.conf  the variable is as default,

 

EXTRA_IMAGE_FEATURES?= “debug-tweaks”

 

Can you please help me to resolve this issue. Please refer the log also.

 

“k2g-evm login: root

login: can't set

Poky (Yocto Project Reference Distro) 3.3+snapshot-f2728d3ec8c0589e02e9a3ce7cf8aca902cae0a3 k2g-evm /dev/ttyS0 “

 

 

Regards

Asif Malek

Assistant Engineer(Delta Electronics India)