A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm using SPI LCD screen as system screen, I wanna rewrite the frame buffer driver, but one thing I could not make clear: What event triggers frame buffer data transfer to LCD? I was told it was done by hardware like LCDC, but still frame buffer needs copy_from_user before an updated data transfer to LCD, so, anybody could tell me how I could rewrite the SPI LCD driver as a standard frame buffer driver? I want to use QT as UI so standard frame buffer driver is needed.
and also, small size LCD uses i8080 interface, that's the same question how to trigger screen write while refreshing the screen.
Best regards,
Pan