Part Number: AM4376
Hi,
My customer reported DDR3L access issue on their board.
The failure is observed more than 10 boards in the market (total 11k boards were released).
The issue happens just after boot-up and the system stops during DDR accesses.
The customer checked the failing boards and found there are differences in DQS signal voltage swing.
On normal boards, the voltage swing is ~700mV (0.684V center).
On failing boards, some DQS signals show voltage swing ~1.344V(0.684V center)
Please see attached excel sheet for waveform comparison in details.
DDR_issue.xlsx
The failing boards show 100% failure rate (i.e. the issue is reproduced 100%).
But these boards were working fine before. Then these boards suddenly showed failing behavior.
Are there any similar issues reported before?
What is potential root cause of the issue?
Any debug recommendation?
Thanks and regards,
Koichiro Tashiro