This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365 DDR2 IF VCLK

In the DDR Interface Description (SPRÙFI2.pdf, march 2009) page 12. Subsection 2.1 says: VCLK is the configuration bus/peripheral system interfaces clock (PLLC1SYSCLK4) wihch then would mena it is programmable. The section 2.1.1 below says : VCLK is clocked at a fixed divider ratio of PLL1. This divider is fixed at 4, that is, VCLK is clocked at a frequency of PLL1/4. What is correct ? Best regards Enst