Hi, I downloaded the WinCE SDK, and installed on the laptop. I programmed a SD card with MLO, ebootsd.nb0, xldruart.nb0, and nk.bin, but the CE booting always stops at the similar location when I tried to boot the AM37x EVM using the provided images in C:\TI\BSP_WINCE_ARM_A8_01_01_00_patch_01\Demo_images\OMAP35XX_AMDM37XX\EBOOT_XLDR. Please let me know how I can fix it. Selection (actual NK from SDCard FILE ): 3 Boot device set to NK from SDCard FILE -------------------------------------------------------------------------------- Main Menu ----------------------------------------------------------- [1] Show Current Settings [2] Select Boot Device [3] Select KITL (Debug) Device [4] Network Settings [5] SDCard Settings [6] Set Device ID [7] Save Settings [8] Flash Management [9] Enable/Disable OAL Retail Messages [a] Select Display Resolution [0] Exit and Continue Selection: 0 Init HW: controller RST SDCARD: reqested speed 1000000, actual speed 1000000 SDCARD: reqested speed 25000000, actual speed 19200000 BLSDCardReadLogo: cannot open Logo.bmp BL_IMAGE_TYPE_BIN Download file information: ----------------------------------------------------------- [0]: Address=0x80002000 Length=0x023c1318 Save=0x80002000 ----------------------------------------------------------- Download file type: 1 ................................................................................ ..ImageStart = 0x80002000, ImageLength = 0x23C1318, LaunchAddr = 0x80012208 Completed file(s): ------------------------------------------------------------------------------- [0]: Address=0x80002000 Length=0x23C1318 Name="" Target=RAM ROMHDR at Address 80002044h Launch Windows CE image by jumping to 0x80012208... Windows CE Kernel for ARM (Thumb Enabled) Built on Aug 4 2010 at 14:23:58 OAL: CPU revision 0x10:DM3730 OAL: CPU L2 Aux register 0x400042 ****Profiler Build**** ---High Performance Frequency is 26000936 hz---