This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UART boot SDRAM allocation problem on C6747

Other Parts Discussed in Thread: TMS320C6747

Hello I have a problem with UART boot. If my project has a code or const allocated in SDRAM, program is not executed properly after UART boot. If SDRAM contains only variables or tables (which do not have to be initialized by the boot program), all goes ok. Maybe my AISGen settings are improper? I use default settings with all checkboxes unchecked. If so, how can I know how to set them? CCSv3.3, Code generation tools v6.1.5, bootloader type D800K003, UART2 boot Device: TMS320C6747, little endian