This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Does the PMIC chip need to communicate with the TDA4VM chip before the PMIC works properly?

Part Number: TDA4VM


That is, does the PMIC chip need to communicate with the TDA4VM chip before PMIC's DC-DCs work?

One of our customized TDA4VM boards is broken, the DC-DCs of PMIC have no output voltage, it was fine before, how to fix it? Thanks.

The PMICs are TPS65941213 and TPS65941111. Only the LDOVINT and LDOVRTC have output voltage, but other LDOs and DC-DCs have no output voltage.

Are the PMICs broken? or Maybe the TDA4VM is broken?

Thanks.

  • Hello,

        The PMIC chips do not need to communicate with the TDA4VM chip.  The PMICs will execute the power up sequence when the ENABLE pin goes high, the VCCA voltage is valid, and there are no residual voltages (>150mV) on any of the regulators.

        Please verify what is broken.  When the PMICs power up, if there are any faults (shorts, residual voltages on rails, no voltage on FB_B3 monitor, etc), then the PMICs will shutdown automatically and attempt a recovery.  After 15 recovery attempts the device will remain in the safe recovery state and require a power cycle.

    (1) Can you verify any rails or GPIO turning on and off the expected 15 times due to an error.  GPIO9 of PMICA and GPIO11 of PMICB are the first two items to be turned on in the sequence.

    (2) While the I2C communication is not needed to start the PMIC this is very valuable to diagnose what is the source of the failure.  The interrupt registers will indicate which regulator the fault occured upon and if the issue was related to OV/UV/SC/ILIM.

    Regards,

    Chris

  • Hello Chris,

       Thanks for your reply.

    Regards,

    Hui