Part Number: AM3354
Other Parts Discussed in Thread: AMIC110
Hi,
About UART register value.
Data Sheets
AM335x and AMIC110 Sitara Processors
Technical Reference Manuals
Universal Asynchronous Receiver/Transmitter (UART)
19.5.1.43 SYSC Register (offset = 54h) [reset = 0h].
The manual says that the value is always 0 when the register is reset.
However, the AUTOIDLE bit is set to 1 even though it is not set software.
Internal interface clock-gating strategy.
0h = Clock is running.
1h = Reserved.
Is there any problem if 1h = Reserved. is set?
Please tell me the meaning of Reserved. if any.
Best Regards,
Jun