This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3358: Can t access PRU with XDS110 on beaglebone black

Part Number: AM3358

Hi,

i'm trying to execute the LAB1 example on the PRU training hands on lab pages, that i downloaded from here.

i followed all the steps, but when i connect to target cortexA8 to execute gel for initialize PRU ICSS, i get this error

CS_DAP_DebugSS: Error: (Error -242 @ 0x0) A router subpath could not be accessed. The board configuration file is probably incorrect. (Emulation package 9.4.0.00129)

and i can't connect to PRU as well.

my test connection on target configuration file works well, and i have powered up the board pressing S2 switch, to prevent boot from linux.

Is this a bug related to emulation package?? Am i doing something wrong? Please give hints

Kind Regards

Emanuele Peruzzi