Other Parts Discussed in Thread: OMAP3530
Hi,
I'm trying to run the readwrite sample program from DSP Link 1.65, but without success.
I followed the instructions on http://processors.wiki.ti.com/index.php/Writing_DSPLink_Application_using_PROC_read_and_write_APIs i.e. I reserved the two regions READMEM and WRITEMEM.
When I try to run the program i get this:
./readwritegpp readwrite.out 2280652800 1024 1
============= Sample Application : READWRITE ==========
Entered RDWR_Create ()
[ 515.812011] Failure [0x8000800b] in [0x401] at line 514
[ 515.817657] Failure [0x8000802d] in [0x401] at line 536
[ 515.823272] Failure [0x8000802d] in [0x401] at line 536
[ 515.828521] Failure [0x8000802d] in [0x401] at line 536
Leaving RDWR_Create ()
Entered RDWR_Execute ()
[ 515.989318] Unable to handle kernel paging request at virtual address 01010105
[ 515.997222] pgd = c5f6c000
[ 515.999938] [01010105] *pgd=00000000
[ 516.003570] Internal error: Oops: 805 [#1]
[ 516.007690] last sysfs file: /sys/devices/virtual/net/lo/flags
[ 516.013549] Modules linked in: lpm_omap3530 dsplinkk
[ 516.018554] CPU: 0 Not tainted (2.6.35.11 #1)
[ 516.023376] PC is at IPS_notify+0x164/0x1f4 [dsplinkk]
[ 516.028533] LR is at __mutex_lock_interruptible_slowpath+0x21c/0x254
[ 516.034942] pc : [<bf005728>] lr : [<c0426de0>] psr: 80000013
[ 516.034942] sp : c5de5e18 ip : 22222222 fp : bec22b9c
[ 516.046478] r10: 00000000 r9 : 01010101 r8 : c8350000
[ 516.051727] r7 : 00000000 r6 : 00000000 r5 : bf033034 r4 : 00008000
[ 516.058288] r3 : 01010101 r2 : 00000000 r1 : 00000000 r0 : 00000000
[ 516.064849] Flags: Nzcv IRQs on FIQs on Mode SVC_32 ISA ARM Segment user
[ 516.072021] Control: 10c5387d Table: 85f6c019 DAC: 00000015
[ 516.077789] Process readwritegpp (pid: 1213, stack limit = 0xc5de42f0)
[ 516.084350] Stack: (0xc5de5e18 to 0xc5de6000)
[ 516.088745] 5e00: c8600000 00000000
[ 516.096954] 5e20: 00000001 02faf080 bec22bac 400d6000 bec22b9c c8600000 bf03393c 00000000
[ 516.105163] 5e40: c838b180 c838b200 bec22bac 400d6000 bec22b9c bf00acb0 00000000 c5de5ef4
[ 516.113403] 5e60: c8600000 c833[<c00cc690>] (sys_ioctl+0x38/0x5c)
[ 516.299255] [<c00cc690>] (sys_ioctl+0x38/0x5c) from [<c0037f00>] (ret_fast_syscall+0x0/0x30)
[ 516.307739] Code: 8a000012 e59d1004 e0893387 e3a02000 (e5831004)
[ 516.314575] ---[ end trace 32dddce6f2a2c647 ]---
I suspect a error in the memory mapping but I can't see what's wrong...
Here are the config files:
Does anybody have a suggestion?
Thanks,
Jonathan