Part Number: PROCESSOR-SDK-AM57X
Other Parts Discussed in Thread: TMDXIDK5718
Hi,
I'm using SDK-LINUX-AM57X 06_03_00_106 on TMDXIDK5718.
I want to convert character code UTF-8 to SHIFT_JIS.
"iconv" is already installed. But it does not contain SHIFT_JIS code.
====
root@am57xx-evm:/tmp# iconv --list
The following list contains all the coded character sets known. This does
not necessarily mean that all combinations of these names can be used for
the FROM and TO command line parameters. One coded character set can be
listed with several different names (aliases).
10646-1:1993, 10646-1:1993/UCS4, ANSI_X3.4-1968, ANSI_X3.4-1986, ANSI_X3.4,
ASCII, CP367, CSASCII, CSUCS4, IBM367, ISO-10646, ISO-10646/UCS2,
ISO-10646/UCS4, ISO-10646/UTF-8, ISO-10646/UTF8, ISO-IR-6, ISO-IR-193,
ISO646-US, ISO_646.IRV:1991, OSF00010020, OSF00010100, OSF00010101,
OSF00010102, OSF00010104, OSF00010105, OSF00010106, OSF05010001, UCS-2,
UCS-2BE, UCS-2LE, UCS-4, UCS-4BE, UCS-4LE, UCS2, UCS4, UNICODEBIG,
UNICODELITTLE, US-ASCII, US, UTF-8, UTF8, WCHAR_T
==
How can I add SHIFT_JIS character code?
Regards,
Toshio Masuchi