PDK: Processor SDK RTOS 06_03_00_106
Dear TI Support Team,
I'm looking into connecting two TMDX654IDKEVM via PCIe. According to the “Processor SDK RTOS 06_03_00_106” (6.1. CSL — Processor SDK RTOS Documentation) in order to connect them together, I need a special MODIFIED male-to-male crossover PCIe x1 or x4 cable.
Unfortunately, the link to the MODIFIED cable in the PDK documentation is broken.
Could you please repair the link or provide here a detailed description of the cable that is required to connect the two boards?
Is it possible to buy this cable directly from TI and if so, what is its part number?
I would be grateful for any information on where to buy the required cable or how to make it by myself.
Thank you in advance!
Kind Regards,
Yury.