Part Number: AM4372
Hi,
We are getting questions from our customers.
They are examining whether a certain QSPI Flash Memory can be used.
It is about the command that ROM Code sends to QSPI when booting from QSPI.
1. Does ROM Code send the commands in the order Enable Reset (66h)-Reset (99h) when it first accesses QSPI?
2. Does the ROM Code leave an interval of 60us or more between the transmission of Reset (99h) and the next command?
Best Regards,
Kouji Nishigata