This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Tftpboot from Ubuntu VM running on Red Hat Host



My environment consists of an Ubuntu 10.04 virtual machine running on a Red Hat 5.4 host.  I have a DM365 EVM, and I am trying to do a tftpboot from the image in the Ubuntu vm.  The following is my setup and the attempt to boot the board:

 

DM365 EVM :>printenv
baudrate=115200
ethaddr=00:0e:99:02:ca:0b
bootdelay=10
env=gatewayip 192.168.1.2
stdin=serial
stdout=serial
stderr=serial
ver=U-Boot 1.3.4 (Mar  2 2009 - 11:50:39)
filesize=1F7640
fileaddr=80700000
netmask=255.255.0.0
ipaddr=192.168.1.4
bootargs=console=ttyS0,115200n8 noinitrd rw ip=192.168.1.4 root=/dev/nfs nfsroot=192.168.185.128:/home/manager/targetfs,nolock mem=76M video=davincifb:vid0=OFF:vid1=OFF:osd0=720x576x16,4050K dm365_imp.oper_mode=0 davinci_capture.device_type=4
bootcmd=dhcp; tftpboot 0x80700000 uImage-dm365-evm.bin; bootm 0x80700000
rootpath=/home/manager/targetfs
bootfile="uImage-dm365-evm.bin"
serverip=192.168.185.128
nfshost=192.168.185.128
gatewayip=192.168.1.2

Environment size: 688/262140 bytes
DM365 EVM :>tftpboot
TFTP from server 192.168.185.128; our IP address is 192.168.1.4
Filename 'uImage-dm365-evm.bin'.
Load address: 0x80700000
Loading: T T

The EVM IP is 192.168.1.4

The Red Hat host IP is 192.168.1.2

The Ubuntu VM IP is 192.168.185.128

I can boot from an image residing on the Red Hat host using a similar configuration.

Can anybody tell me how to get the boot image from the VM?