Part Number: TDA4VM
Customer is considering to encode a processed RADAR signal for transmission. It would be a single bit stream of 12-bit samples. They realize it would not be lossless.
1) Would it work to use one of the planar formats and fill the Y-buffer with the radar data and U/V buffer with zero data? In other words, does it process the luma and chroma channels independently or would providing dummy zero data to U/V channel have a negative impact on the encoded Y stream?
2) Table 6693 in TRM mentions 10-bit formats " unless the hardware doesn't support 10-bit pipeline". Does encoder instantiation on TDA4VM support 10-bit pipeline? And I assume that 12-bit sample stream is definitely not supported?
3) Any general comments on this application to guide customer? has anyone seen H.264 used to encode non-video data, etc
Thanks,
David