Other Parts Discussed in Thread: DP83869
Hi All,
I am using dual "BCM54616S" Broadcom 10/100/1000 Phy chip with the copper interface with AM335x based controller. Trying to migrate from Broadcom Copper PHY chip to a TI DP83869 Phy chip 100BASE-FX Fiber.
For the same, I have made changes in U-Boot, Linux Kernel and DTB
In U-Boot,
1. Disabled auto-negotiation in 'macb.c' file. Attached File for reference
2. Added 'DP83869' driver files and edited makefile. u-boot\drivers\net\phy\dp83869.c, u-boot/include/dt-bindings/net/ti-dp83869.h
3. Edited PHY address in 'cpsw_slaves' structure.
{
.slave_reg_ofs = 0x208,
.sliver_reg_ofs = 0xd80,
.phy_addr = 10,
},
{
.slave_reg_ofs = 0x308,
.sliver_reg_ofs = 0xdc0,
.phy_addr = 11,
},
};
Changes done in u-boot\arch\arm\dts\am335x-evm.dts
&cpsw_emac0 {
phy_id = <&davinci_mdio>, <10>;
phy-mode = "rgmii-txid";
dual_emac_res_vlan = <1>;
};
&cpsw_emac1 {
phy_id = <&davinci_mdio>, <11>;
phy-mode = "rgmii-txid";
dual_emac_res_vlan = <2>;
};
/* * Copyright (C) 2005-2006 Atmel Corporation * * SPDX-License-Identifier: GPL-2.0+ */ #include <common.h> #include <clk.h> #include <dm.h> /* * The u-boot networking stack is a little weird. It seems like the * networking core allocates receive buffers up front without any * regard to the hardware that's supposed to actually receive those * packets. * * The MACB receives packets into 128-byte receive buffers, so the * buffers allocated by the core isn't very practical to use. We'll * allocate our own, but we need one such buffer in case a packet * wraps around the DMA ring so that we have to copy it. * * Therefore, define CONFIG_SYS_RX_ETH_BUFFER to 1 in the board-specific * configuration header. This way, the core allocates one RX buffer * and one TX buffer, each of which can hold a ethernet packet of * maximum size. * * For some reason, the networking core unconditionally specifies a * 32-byte packet "alignment" (which really should be called * "padding"). MACB shouldn't need that, but we'll refrain from any * core modifications here... */ #include <net.h> #ifndef CONFIG_DM_ETH #include <netdev.h> #endif #include <malloc.h> #include <miiphy.h> #include <linux/mii.h> #include <asm/io.h> #include <asm/dma-mapping.h> #include <asm/arch/clk.h> #include <linux/errno.h> #include "macb.h" DECLARE_GLOBAL_DATA_PTR; #define MACB_RX_BUFFER_SIZE 4096 #define MACB_RX_RING_SIZE (MACB_RX_BUFFER_SIZE / 128) #define MACB_TX_RING_SIZE 16 #define MACB_TX_TIMEOUT 1000 #define MACB_AUTONEG_TIMEOUT 5000000 struct macb_dma_desc { u32 addr; u32 ctrl; }; #define DMA_DESC_BYTES(n) (n * sizeof(struct macb_dma_desc)) #define MACB_TX_DMA_DESC_SIZE (DMA_DESC_BYTES(MACB_TX_RING_SIZE)) #define MACB_RX_DMA_DESC_SIZE (DMA_DESC_BYTES(MACB_RX_RING_SIZE)) #define MACB_TX_DUMMY_DMA_DESC_SIZE (DMA_DESC_BYTES(1)) #define RXADDR_USED 0x00000001 #define RXADDR_WRAP 0x00000002 #define RXBUF_FRMLEN_MASK 0x00000fff #define RXBUF_FRAME_START 0x00004000 #define RXBUF_FRAME_END 0x00008000 #define RXBUF_TYPEID_MATCH 0x00400000 #define RXBUF_ADDR4_MATCH 0x00800000 #define RXBUF_ADDR3_MATCH 0x01000000 #define RXBUF_ADDR2_MATCH 0x02000000 #define RXBUF_ADDR1_MATCH 0x04000000 #define RXBUF_BROADCAST 0x80000000 #define TXBUF_FRMLEN_MASK 0x000007ff #define TXBUF_FRAME_END 0x00008000 #define TXBUF_NOCRC 0x00010000 #define TXBUF_EXHAUSTED 0x08000000 #define TXBUF_UNDERRUN 0x10000000 #define TXBUF_MAXRETRY 0x20000000 #define TXBUF_WRAP 0x40000000 #define TXBUF_USED 0x80000000 struct macb_device { void *regs; unsigned int rx_tail; unsigned int tx_head; unsigned int tx_tail; unsigned int next_rx_tail; bool wrapped; void *rx_buffer; void *tx_buffer; struct macb_dma_desc *rx_ring; struct macb_dma_desc *tx_ring; unsigned long rx_buffer_dma; unsigned long rx_ring_dma; unsigned long tx_ring_dma; struct macb_dma_desc *dummy_desc; unsigned long dummy_desc_dma; const struct device *dev; #ifndef CONFIG_DM_ETH struct eth_device netdev; #endif unsigned short phy_addr; struct mii_dev *bus; #ifdef CONFIG_PHYLIB struct phy_device *phydev; #endif #ifdef CONFIG_DM_ETH #ifdef CONFIG_CLK unsigned long pclk_rate; #endif phy_interface_t phy_interface; #endif }; #ifndef CONFIG_DM_ETH #define to_macb(_nd) container_of(_nd, struct macb_device, netdev) #endif static int macb_is_gem(struct macb_device *macb) { return MACB_BFEXT(IDNUM, macb_readl(macb, MID)) == 0x2; } #ifndef cpu_is_sama5d2 #define cpu_is_sama5d2() 0 #endif #ifndef cpu_is_sama5d4 #define cpu_is_sama5d4() 0 #endif static int gem_is_gigabit_capable(struct macb_device *macb) { /* * The GEM controllers embedded in SAMA5D2 and SAMA5D4 are * configured to support only 10/100. */ return macb_is_gem(macb) && !cpu_is_sama5d2() && !cpu_is_sama5d4(); } static void macb_mdio_write(struct macb_device *macb, u8 reg, u16 value) { unsigned long netctl; unsigned long netstat; unsigned long frame; netctl = macb_readl(macb, NCR); netctl |= MACB_BIT(MPE); macb_writel(macb, NCR, netctl); frame = (MACB_BF(SOF, 1) | MACB_BF(RW, 1) | MACB_BF(PHYA, macb->phy_addr) | MACB_BF(REGA, reg) | MACB_BF(CODE, 2) | MACB_BF(DATA, value)); macb_writel(macb, MAN, frame); do { netstat = macb_readl(macb, NSR); } while (!(netstat & MACB_BIT(IDLE))); netctl = macb_readl(macb, NCR); netctl &= ~MACB_BIT(MPE); macb_writel(macb, NCR, netctl); } static u16 macb_mdio_read(struct macb_device *macb, u8 reg) { unsigned long netctl; unsigned long netstat; unsigned long frame; netctl = macb_readl(macb, NCR); netctl |= MACB_BIT(MPE); macb_writel(macb, NCR, netctl); frame = (MACB_BF(SOF, 1) | MACB_BF(RW, 2) | MACB_BF(PHYA, macb->phy_addr) | MACB_BF(REGA, reg) | MACB_BF(CODE, 2)); macb_writel(macb, MAN, frame); do { netstat = macb_readl(macb, NSR); } while (!(netstat & MACB_BIT(IDLE))); frame = macb_readl(macb, MAN); netctl = macb_readl(macb, NCR); netctl &= ~MACB_BIT(MPE); macb_writel(macb, NCR, netctl); return MACB_BFEXT(DATA, frame); } void __weak arch_get_mdio_control(const char *name) { return; } #if defined(CONFIG_CMD_MII) || defined(CONFIG_PHYLIB) int macb_miiphy_read(struct mii_dev *bus, int phy_adr, int devad, int reg) { u16 value = 0; #ifdef CONFIG_DM_ETH struct udevice *dev = eth_get_dev_by_name(bus->name); struct macb_device *macb = dev_get_priv(dev); #else struct eth_device *dev = eth_get_dev_by_name(bus->name); struct macb_device *macb = to_macb(dev); #endif if (macb->phy_addr != phy_adr) return -1; arch_get_mdio_control(bus->name); value = macb_mdio_read(macb, reg); return value; } int macb_miiphy_write(struct mii_dev *bus, int phy_adr, int devad, int reg, u16 value) { #ifdef CONFIG_DM_ETH struct udevice *dev = eth_get_dev_by_name(bus->name); struct macb_device *macb = dev_get_priv(dev); #else struct eth_device *dev = eth_get_dev_by_name(bus->name); struct macb_device *macb = to_macb(dev); #endif if (macb->phy_addr != phy_adr) return -1; arch_get_mdio_control(bus->name); macb_mdio_write(macb, reg, value); return 0; } #endif #define RX 1 #define TX 0 static inline void macb_invalidate_ring_desc(struct macb_device *macb, bool rx) { if (rx) invalidate_dcache_range(macb->rx_ring_dma, ALIGN(macb->rx_ring_dma + MACB_RX_DMA_DESC_SIZE, PKTALIGN)); else invalidate_dcache_range(macb->tx_ring_dma, ALIGN(macb->tx_ring_dma + MACB_TX_DMA_DESC_SIZE, PKTALIGN)); } static inline void macb_flush_ring_desc(struct macb_device *macb, bool rx) { if (rx) flush_dcache_range(macb->rx_ring_dma, macb->rx_ring_dma + ALIGN(MACB_RX_DMA_DESC_SIZE, PKTALIGN)); else flush_dcache_range(macb->tx_ring_dma, macb->tx_ring_dma + ALIGN(MACB_TX_DMA_DESC_SIZE, PKTALIGN)); } static inline void macb_flush_rx_buffer(struct macb_device *macb) { flush_dcache_range(macb->rx_buffer_dma, macb->rx_buffer_dma + ALIGN(MACB_RX_BUFFER_SIZE, PKTALIGN)); } static inline void macb_invalidate_rx_buffer(struct macb_device *macb) { invalidate_dcache_range(macb->rx_buffer_dma, macb->rx_buffer_dma + ALIGN(MACB_RX_BUFFER_SIZE, PKTALIGN)); } #if defined(CONFIG_CMD_NET) static int _macb_send(struct macb_device *macb, const char *name, void *packet, int length) { unsigned long paddr, ctrl; unsigned int tx_head = macb->tx_head; int i; paddr = dma_map_single(packet, length, DMA_TO_DEVICE); ctrl = length & TXBUF_FRMLEN_MASK; ctrl |= TXBUF_FRAME_END; if (tx_head == (MACB_TX_RING_SIZE - 1)) { ctrl |= TXBUF_WRAP; macb->tx_head = 0; } else { macb->tx_head++; } macb->tx_ring[tx_head].ctrl = ctrl; macb->tx_ring[tx_head].addr = paddr; barrier(); macb_flush_ring_desc(macb, TX); /* Do we need check paddr and length is dcache line aligned? */ flush_dcache_range(paddr, paddr + ALIGN(length, ARCH_DMA_MINALIGN)); macb_writel(macb, NCR, MACB_BIT(TE) | MACB_BIT(RE) | MACB_BIT(TSTART)); /* * I guess this is necessary because the networking core may * re-use the transmit buffer as soon as we return... */ for (i = 0; i <= MACB_TX_TIMEOUT; i++) { barrier(); macb_invalidate_ring_desc(macb, TX); ctrl = macb->tx_ring[tx_head].ctrl; if (ctrl & TXBUF_USED) break; udelay(1); } dma_unmap_single(packet, length, paddr); if (i <= MACB_TX_TIMEOUT) { if (ctrl & TXBUF_UNDERRUN) printf("%s: TX underrun\n", name); if (ctrl & TXBUF_EXHAUSTED) printf("%s: TX buffers exhausted in mid frame\n", name); } else { printf("%s: TX timeout\n", name); } /* No one cares anyway */ return 0; } static void reclaim_rx_buffers(struct macb_device *macb, unsigned int new_tail) { unsigned int i; i = macb->rx_tail; macb_invalidate_ring_desc(macb, RX); while (i > new_tail) { macb->rx_ring[i].addr &= ~RXADDR_USED; i++; if (i > MACB_RX_RING_SIZE) i = 0; } while (i < new_tail) { macb->rx_ring[i].addr &= ~RXADDR_USED; i++; } barrier(); macb_flush_ring_desc(macb, RX); macb->rx_tail = new_tail; } static int _macb_recv(struct macb_device *macb, uchar **packetp) { unsigned int next_rx_tail = macb->next_rx_tail; void *buffer; int length; u32 status; macb->wrapped = false; for (;;) { macb_invalidate_ring_desc(macb, RX); if (!(macb->rx_ring[next_rx_tail].addr & RXADDR_USED)) return -EAGAIN; status = macb->rx_ring[next_rx_tail].ctrl; if (status & RXBUF_FRAME_START) { if (next_rx_tail != macb->rx_tail) reclaim_rx_buffers(macb, next_rx_tail); macb->wrapped = false; } if (status & RXBUF_FRAME_END) { buffer = macb->rx_buffer + 128 * macb->rx_tail; length = status & RXBUF_FRMLEN_MASK; macb_invalidate_rx_buffer(macb); if (macb->wrapped) { unsigned int headlen, taillen; headlen = 128 * (MACB_RX_RING_SIZE - macb->rx_tail); taillen = length - headlen; memcpy((void *)net_rx_packets[0], buffer, headlen); memcpy((void *)net_rx_packets[0] + headlen, macb->rx_buffer, taillen); *packetp = (void *)net_rx_packets[0]; } else { *packetp = buffer; } if (++next_rx_tail >= MACB_RX_RING_SIZE) next_rx_tail = 0; macb->next_rx_tail = next_rx_tail; return length; } else { if (++next_rx_tail >= MACB_RX_RING_SIZE) { macb->wrapped = true; next_rx_tail = 0; } } barrier(); } } static void macb_phy_reset(struct macb_device *macb, const char *name) { int i; u16 status, adv; adv = ADVERTISE_CSMA | ADVERTISE_ALL; macb_mdio_write(macb, MII_ADVERTISE, adv); macb_mdio_write(macb, MII_BMCR,(BMCR_SPEED100 | BMCR_FULLDPLX)); printf(" macb_phy_reset \n"); #if 0 printf("%s: Starting autonegotiation...\n", name); macb_mdio_write(macb, MII_BMCR, (BMCR_ANENABLE | BMCR_ANRESTART)); for (i = 0; i < MACB_AUTONEG_TIMEOUT / 100; i++) { status = macb_mdio_read(macb, MII_BMSR); if (status & BMSR_ANEGCOMPLETE) break; udelay(100); } if (status & BMSR_ANEGCOMPLETE) printf("%s: Autonegotiation complete\n", name); else printf("%s: Autonegotiation timed out (status=0x%04x)\n", name, status); #endif } static int macb_phy_find(struct macb_device *macb, const char *name) { int i; u16 phy_id; /* Search for PHY... */ for (i = 0; i < 32; i++) { macb->phy_addr = i; phy_id = macb_mdio_read(macb, MII_PHYSID1); if (phy_id != 0xffff) { printf("%s: PHY present at %d\n", name, i); return 1; } } /* PHY isn't up to snuff */ printf("%s: PHY not found\n", name); return 0; } #ifdef CONFIG_DM_ETH static int macb_phy_init(struct udevice *dev, const char *name) #else static int macb_phy_init(struct macb_device *macb, const char *name) #endif { #ifdef CONFIG_DM_ETH struct macb_device *macb = dev_get_priv(dev); #endif u32 ncfgr; u16 phy_id, status, adv, lpa; int media, speed, duplex; int i; arch_get_mdio_control(name); /* Auto-detect phy_addr */ if (!macb_phy_find(macb, name)) return 0; /* Check if the PHY is up to snuff... */ phy_id = macb_mdio_read(macb, MII_PHYSID1); if (phy_id == 0xffff) { printf("%s: No PHY present\n", name); return 0; } #ifdef CONFIG_PHYLIB #ifdef CONFIG_DM_ETH macb->phydev = phy_connect(macb->bus, macb->phy_addr, dev, macb->phy_interface); #else /* need to consider other phy interface mode */ macb->phydev = phy_connect(macb->bus, macb->phy_addr, &macb->netdev, PHY_INTERFACE_MODE_RGMII); #endif if (!macb->phydev) { printf("phy_connect failed\n"); return -ENODEV; } phy_config(macb->phydev); #endif status = macb_mdio_read(macb, MII_BMSR); if (!(status & BMSR_LSTATUS)) { /* Try to re-negotiate if we don't have link already. */ macb_phy_reset(macb, name); for (i = 0; i < MACB_AUTONEG_TIMEOUT / 100; i++) { status = macb_mdio_read(macb, MII_BMSR); if (status & BMSR_LSTATUS) break; udelay(100); } } if (!(status & BMSR_LSTATUS)) { printf("%s: link down (status: 0x%04x)\n", name, status); return 0; } /* First check for GMAC and that it is GiB capable */ if (gem_is_gigabit_capable(macb)) { lpa = macb_mdio_read(macb, MII_STAT1000); if (lpa & (LPA_1000FULL | LPA_1000HALF)) { duplex = ((lpa & LPA_1000FULL) ? 1 : 0); printf("%s: link up, 1000Mbps %s-duplex (lpa: 0x%04x)\n", name, duplex ? "full" : "half", lpa); ncfgr = macb_readl(macb, NCFGR); ncfgr &= ~(MACB_BIT(SPD) | MACB_BIT(FD)); ncfgr |= GEM_BIT(GBE); if (duplex) ncfgr |= MACB_BIT(FD); macb_writel(macb, NCFGR, ncfgr); return 1; } } /* fall back for EMAC checking */ adv = macb_mdio_read(macb, MII_ADVERTISE); lpa = macb_mdio_read(macb, MII_LPA); media = mii_nway_result(lpa & adv); speed = (media & (ADVERTISE_100FULL | ADVERTISE_100HALF) ? 1 : 0); duplex = (media & ADVERTISE_FULL) ? 1 : 0; printf("%s: link up, %sMbps %s-duplex (lpa: 0x%04x)\n", name, speed ? "100" : "10", duplex ? "full" : "half", lpa); ncfgr = macb_readl(macb, NCFGR); ncfgr &= ~(MACB_BIT(SPD) | MACB_BIT(FD) | GEM_BIT(GBE)); if (speed) ncfgr |= MACB_BIT(SPD); if (duplex) ncfgr |= MACB_BIT(FD); macb_writel(macb, NCFGR, ncfgr); return 1; } static int gmac_init_multi_queues(struct macb_device *macb) { int i, num_queues = 1; u32 queue_mask; /* bit 0 is never set but queue 0 always exists */ queue_mask = gem_readl(macb, DCFG6) & 0xff; queue_mask |= 0x1; for (i = 1; i < MACB_MAX_QUEUES; i++) if (queue_mask & (1 << i)) num_queues++; macb->dummy_desc->ctrl = TXBUF_USED; macb->dummy_desc->addr = 0; flush_dcache_range(macb->dummy_desc_dma, macb->dummy_desc_dma + ALIGN(MACB_TX_DUMMY_DMA_DESC_SIZE, PKTALIGN)); for (i = 1; i < num_queues; i++) gem_writel_queue_TBQP(macb, macb->dummy_desc_dma, i - 1); return 0; } #ifdef CONFIG_DM_ETH static int _macb_init(struct udevice *dev, const char *name) #else static int _macb_init(struct macb_device *macb, const char *name) #endif { #ifdef CONFIG_DM_ETH struct macb_device *macb = dev_get_priv(dev); #endif unsigned long paddr; int i; /* * macb_halt should have been called at some point before now, * so we'll assume the controller is idle. */ /* initialize DMA descriptors */ paddr = macb->rx_buffer_dma; for (i = 0; i < MACB_RX_RING_SIZE; i++) { if (i == (MACB_RX_RING_SIZE - 1)) paddr |= RXADDR_WRAP; macb->rx_ring[i].addr = paddr; macb->rx_ring[i].ctrl = 0; paddr += 128; } macb_flush_ring_desc(macb, RX); macb_flush_rx_buffer(macb); for (i = 0; i < MACB_TX_RING_SIZE; i++) { macb->tx_ring[i].addr = 0; if (i == (MACB_TX_RING_SIZE - 1)) macb->tx_ring[i].ctrl = TXBUF_USED | TXBUF_WRAP; else macb->tx_ring[i].ctrl = TXBUF_USED; } macb_flush_ring_desc(macb, TX); macb->rx_tail = 0; macb->tx_head = 0; macb->tx_tail = 0; macb->next_rx_tail = 0; macb_writel(macb, RBQP, macb->rx_ring_dma); macb_writel(macb, TBQP, macb->tx_ring_dma); if (macb_is_gem(macb)) { /* Check the multi queue and initialize the queue for tx */ gmac_init_multi_queues(macb); /* * When the GMAC IP with GE feature, this bit is used to * select interface between RGMII and GMII. * When the GMAC IP without GE feature, this bit is used * to select interface between RMII and MII. */ #ifdef CONFIG_DM_ETH if ((macb->phy_interface == PHY_INTERFACE_MODE_RMII) || (macb->phy_interface == PHY_INTERFACE_MODE_RGMII)) gem_writel(macb, UR, GEM_BIT(RGMII)); else gem_writel(macb, UR, 0); #else #if defined(CONFIG_RGMII) || defined(CONFIG_RMII) gem_writel(macb, UR, GEM_BIT(RGMII)); #else gem_writel(macb, UR, 0); #endif #endif } else { /* choose RMII or MII mode. This depends on the board */ #ifdef CONFIG_DM_ETH #ifdef CONFIG_AT91FAMILY if (macb->phy_interface == PHY_INTERFACE_MODE_RMII) { macb_writel(macb, USRIO, MACB_BIT(RMII) | MACB_BIT(CLKEN)); } else { macb_writel(macb, USRIO, MACB_BIT(CLKEN)); } #else if (macb->phy_interface == PHY_INTERFACE_MODE_RMII) macb_writel(macb, USRIO, 0); else macb_writel(macb, USRIO, MACB_BIT(MII)); #endif #else #ifdef CONFIG_RMII #ifdef CONFIG_AT91FAMILY macb_writel(macb, USRIO, MACB_BIT(RMII) | MACB_BIT(CLKEN)); #else macb_writel(macb, USRIO, 0); #endif #else #ifdef CONFIG_AT91FAMILY macb_writel(macb, USRIO, MACB_BIT(CLKEN)); #else macb_writel(macb, USRIO, MACB_BIT(MII)); #endif #endif /* CONFIG_RMII */ #endif } #ifdef CONFIG_DM_ETH if (!macb_phy_init(dev, name)) #else if (!macb_phy_init(macb, name)) #endif return -1; /* Enable TX and RX */ macb_writel(macb, NCR, MACB_BIT(TE) | MACB_BIT(RE)); return 0; } static void _macb_halt(struct macb_device *macb) { u32 ncr, tsr; /* Halt the controller and wait for any ongoing transmission to end. */ ncr = macb_readl(macb, NCR); ncr |= MACB_BIT(THALT); macb_writel(macb, NCR, ncr); do { tsr = macb_readl(macb, TSR); } while (tsr & MACB_BIT(TGO)); /* Disable TX and RX, and clear statistics */ macb_writel(macb, NCR, MACB_BIT(CLRSTAT)); } static int _macb_write_hwaddr(struct macb_device *macb, unsigned char *enetaddr) { u32 hwaddr_bottom; u16 hwaddr_top; /* set hardware address */ hwaddr_bottom = enetaddr[0] | enetaddr[1] << 8 | enetaddr[2] << 16 | enetaddr[3] << 24; macb_writel(macb, SA1B, hwaddr_bottom); hwaddr_top = enetaddr[4] | enetaddr[5] << 8; macb_writel(macb, SA1T, hwaddr_top); return 0; } static u32 macb_mdc_clk_div(int id, struct macb_device *macb) { u32 config; #if defined(CONFIG_DM_ETH) && defined(CONFIG_CLK) unsigned long macb_hz = macb->pclk_rate; #else unsigned long macb_hz = get_macb_pclk_rate(id); #endif if (macb_hz < 20000000) config = MACB_BF(CLK, MACB_CLK_DIV8); else if (macb_hz < 40000000) config = MACB_BF(CLK, MACB_CLK_DIV16); else if (macb_hz < 80000000) config = MACB_BF(CLK, MACB_CLK_DIV32); else config = MACB_BF(CLK, MACB_CLK_DIV64); return config; } static u32 gem_mdc_clk_div(int id, struct macb_device *macb) { u32 config; #if defined(CONFIG_DM_ETH) && defined(CONFIG_CLK) unsigned long macb_hz = macb->pclk_rate; #else unsigned long macb_hz = get_macb_pclk_rate(id); #endif if (macb_hz < 20000000) config = GEM_BF(CLK, GEM_CLK_DIV8); else if (macb_hz < 40000000) config = GEM_BF(CLK, GEM_CLK_DIV16); else if (macb_hz < 80000000) config = GEM_BF(CLK, GEM_CLK_DIV32); else if (macb_hz < 120000000) config = GEM_BF(CLK, GEM_CLK_DIV48); else if (macb_hz < 160000000) config = GEM_BF(CLK, GEM_CLK_DIV64); else config = GEM_BF(CLK, GEM_CLK_DIV96); return config; } /* * Get the DMA bus width field of the network configuration register that we * should program. We find the width from decoding the design configuration * register to find the maximum supported data bus width. */ static u32 macb_dbw(struct macb_device *macb) { switch (GEM_BFEXT(DBWDEF, gem_readl(macb, DCFG1))) { case 4: return GEM_BF(DBW, GEM_DBW128); case 2: return GEM_BF(DBW, GEM_DBW64); case 1: default: return GEM_BF(DBW, GEM_DBW32); } } static void _macb_eth_initialize(struct macb_device *macb) { int id = 0; /* This is not used by functions we call */ u32 ncfgr; /* TODO: we need check the rx/tx_ring_dma is dcache line aligned */ macb->rx_buffer = dma_alloc_coherent(MACB_RX_BUFFER_SIZE, &macb->rx_buffer_dma); macb->rx_ring = dma_alloc_coherent(MACB_RX_DMA_DESC_SIZE, &macb->rx_ring_dma); macb->tx_ring = dma_alloc_coherent(MACB_TX_DMA_DESC_SIZE, &macb->tx_ring_dma); macb->dummy_desc = dma_alloc_coherent(MACB_TX_DUMMY_DMA_DESC_SIZE, &macb->dummy_desc_dma); /* * Do some basic initialization so that we at least can talk * to the PHY */ if (macb_is_gem(macb)) { ncfgr = gem_mdc_clk_div(id, macb); ncfgr |= macb_dbw(macb); } else { ncfgr = macb_mdc_clk_div(id, macb); } macb_writel(macb, NCFGR, ncfgr); } #ifndef CONFIG_DM_ETH static int macb_send(struct eth_device *netdev, void *packet, int length) { struct macb_device *macb = to_macb(netdev); return _macb_send(macb, netdev->name, packet, length); } static int macb_recv(struct eth_device *netdev) { struct macb_device *macb = to_macb(netdev); uchar *packet; int length; macb->wrapped = false; for (;;) { macb->next_rx_tail = macb->rx_tail; length = _macb_recv(macb, &packet); if (length >= 0) { net_process_received_packet(packet, length); reclaim_rx_buffers(macb, macb->next_rx_tail); } else if (length < 0) { return length; } } } static int macb_init(struct eth_device *netdev, bd_t *bd) { struct macb_device *macb = to_macb(netdev); return _macb_init(macb, netdev->name); } static void macb_halt(struct eth_device *netdev) { struct macb_device *macb = to_macb(netdev); return _macb_halt(macb); } static int macb_write_hwaddr(struct eth_device *netdev) { struct macb_device *macb = to_macb(netdev); return _macb_write_hwaddr(macb, netdev->enetaddr); } int macb_eth_initialize(int id, void *regs, unsigned int phy_addr) { struct macb_device *macb; struct eth_device *netdev; macb = malloc(sizeof(struct macb_device)); if (!macb) { printf("Error: Failed to allocate memory for MACB%d\n", id); return -1; } memset(macb, 0, sizeof(struct macb_device)); netdev = &macb->netdev; macb->regs = regs; macb->phy_addr = phy_addr; if (macb_is_gem(macb)) sprintf(netdev->name, "gmac%d", id); else sprintf(netdev->name, "macb%d", id); netdev->init = macb_init; netdev->halt = macb_halt; netdev->send = macb_send; netdev->recv = macb_recv; netdev->write_hwaddr = macb_write_hwaddr; _macb_eth_initialize(macb); eth_register(netdev); #if defined(CONFIG_CMD_MII) || defined(CONFIG_PHYLIB) int retval; struct mii_dev *mdiodev = mdio_alloc(); if (!mdiodev) return -ENOMEM; strncpy(mdiodev->name, netdev->name, MDIO_NAME_LEN); mdiodev->read = macb_miiphy_read; mdiodev->write = macb_miiphy_write; retval = mdio_register(mdiodev); if (retval < 0) return retval; macb->bus = miiphy_get_dev_by_name(netdev->name); #endif return 0; } #endif /* !CONFIG_DM_ETH */ #ifdef CONFIG_DM_ETH static int macb_start(struct udevice *dev) { return _macb_init(dev, dev->name); } static int macb_send(struct udevice *dev, void *packet, int length) { struct macb_device *macb = dev_get_priv(dev); return _macb_send(macb, dev->name, packet, length); } static int macb_recv(struct udevice *dev, int flags, uchar **packetp) { struct macb_device *macb = dev_get_priv(dev); macb->next_rx_tail = macb->rx_tail; macb->wrapped = false; return _macb_recv(macb, packetp); } static int macb_free_pkt(struct udevice *dev, uchar *packet, int length) { struct macb_device *macb = dev_get_priv(dev); reclaim_rx_buffers(macb, macb->next_rx_tail); return 0; } static void macb_stop(struct udevice *dev) { struct macb_device *macb = dev_get_priv(dev); _macb_halt(macb); } static int macb_write_hwaddr(struct udevice *dev) { struct eth_pdata *plat = dev_get_platdata(dev); struct macb_device *macb = dev_get_priv(dev); return _macb_write_hwaddr(macb, plat->enetaddr); } static const struct eth_ops macb_eth_ops = { .start = macb_start, .send = macb_send, .recv = macb_recv, .stop = macb_stop, .free_pkt = macb_free_pkt, .write_hwaddr = macb_write_hwaddr, }; #ifdef CONFIG_CLK static int macb_enable_clk(struct udevice *dev) { struct macb_device *macb = dev_get_priv(dev); struct clk clk; ulong clk_rate; int ret; ret = clk_get_by_index(dev, 0, &clk); if (ret) return -EINVAL; ret = clk_enable(&clk); if (ret) return ret; clk_rate = clk_get_rate(&clk); if (!clk_rate) return -EINVAL; macb->pclk_rate = clk_rate; return 0; } #endif static int macb_eth_probe(struct udevice *dev) { struct eth_pdata *pdata = dev_get_platdata(dev); struct macb_device *macb = dev_get_priv(dev); const char *phy_mode; __maybe_unused int ret; phy_mode = fdt_getprop(gd->fdt_blob, dev_of_offset(dev), "phy-mode", NULL); if (phy_mode) macb->phy_interface = phy_get_interface_by_name(phy_mode); if (macb->phy_interface == -1) { debug("%s: Invalid PHY interface '%s'\n", __func__, phy_mode); return -EINVAL; } macb->regs = (void *)pdata->iobase; #ifdef CONFIG_CLK ret = macb_enable_clk(dev); if (ret) return ret; #endif _macb_eth_initialize(macb); #if defined(CONFIG_CMD_MII) || defined(CONFIG_PHYLIB) macb->bus = mdio_alloc(); if (!macb->bus) return -ENOMEM; strncpy(macb->bus->name, dev->name, MDIO_NAME_LEN); macb->bus->read = macb_miiphy_read; macb->bus->write = macb_miiphy_write; ret = mdio_register(macb->bus); if (ret < 0) return ret; macb->bus = miiphy_get_dev_by_name(dev->name); #endif return 0; } static int macb_eth_remove(struct udevice *dev) { struct macb_device *macb = dev_get_priv(dev); #ifdef CONFIG_PHYLIB free(macb->phydev); #endif mdio_unregister(macb->bus); mdio_free(macb->bus); return 0; } static int macb_eth_ofdata_to_platdata(struct udevice *dev) { struct eth_pdata *pdata = dev_get_platdata(dev); pdata->iobase = devfdt_get_addr(dev); return 0; } static const struct udevice_id macb_eth_ids[] = { { .compatible = "cdns,macb" }, { .compatible = "cdns,at91sam9260-macb" }, { .compatible = "atmel,sama5d2-gem" }, { .compatible = "atmel,sama5d3-gem" }, { .compatible = "atmel,sama5d4-gem" }, { } }; U_BOOT_DRIVER(eth_macb) = { .name = "eth_macb", .id = UCLASS_ETH, .of_match = macb_eth_ids, .ofdata_to_platdata = macb_eth_ofdata_to_platdata, .probe = macb_eth_probe, .remove = macb_eth_remove, .ops = &macb_eth_ops, .priv_auto_alloc_size = sizeof(struct macb_device), .platdata_auto_alloc_size = sizeof(struct eth_pdata), }; #endif #endif
U-Boot SPL 2018.01-00444-g96cdbef-dirty (Sep 17 2021 - 16:43:52) Trying to boot from UART CCCxyzModem - CRC mode, 2(SOH)/623(STX)/0(CAN) packets, 5 retries Loaded 637268 bytes U-Boot 2018.01-00444-g96cdbef-dirty (Sep 17 2021 - 16:43:52 +0530) Model: TI AM335x EVM DRAM: 256 MiB NAND: 256 MiB MMC: OMAP SD/MMC: 0 ** Bad device mmc 0 ** Using default environment <ethaddr> not set. Validating first E-fuse MAC Net: Could not get PHY for cpsw: addr 10 cpsw, usb_ether Hit any key to stop autoboot: 0 ## Error: "update_to_fit" not defined ## Error: "findfdt" not defined ## Error: "init_console" not defined ## Error: "envboot" not defined ## Error: "distro_bootcmd" not defined
Still Fiber connectivity is not through. TFTP connection is not getting succeeded in U-BOOT.
Details of code changes and U boot error logs attached.
Appreciate if anyone can share documentation describing the software (U-Boot, Linux Kernel(4.14.67) and DTB ) changes for TI DP83869 Phy chip integration.
Regards
Shanid