Part Number: AM6441
Hello TI team,
The newest design I'm developing is based on AM6441 Sitara Processor. At the moment I have to provide to our EMS the exact part number to mount on my PCBs, and I have a couple of questions in order to define it:
- In the field "f" of the nomenclature I have to choose between value E (ICSS + EtherCAT HW Accelerator + CAN-FD Enabled) and F (ICSS + EtherCAT HW Accelerator + CAN-FD + Pre-integrated Stacks Enabled) but I have no idea about what advantage could I have if I choose the pre-integrated stack option.
- Similar to the previous point, but regarding field y "Functional safety". If I mount a non-functional safety device, which features do I loose or which risks can I possibly face?
- Once in the field y "Security" I choose H (i.e HS device and not a GP device), I know there are two sub-types for high secure devices, the Field Securable (FS) and the Security Enforced (SE). How can I select one of them in the part number?
So said, can you check if I correctly understood the nomenclature? See below:
AM6441ASEFHAALV: it means AM6441 device , speed grade 1GHz for A53SS , ICSS + CAN-FD enabled, functional-safe, security (HS device)
AM6441ASEFGAALV: it means AM6441 device , speed grade 1GHz for A53SS , ICSS + CAN-FD enabled, functional-safe, no security (GP device)
Is it right?
Thank you for your help.
Flavio