Part Number: AM3352
Other Parts Discussed in Thread: AM3359
My customer is using CCS to debug the AM3352 via the XDS200.
Timer interrupt behavior does not work well.
When they created the SYS/BIOS Timer by Add on app.cfg and started debugging with the XDS200
it does not stop with the main function.
If you do not use the above and create it in their source code,
The Timer create function displays ADP_stopped exception 0x801*** in the Console and does not work.
In case the first argument of Timer_create is Timer_any, they have above situation.
In case they increase the number, The return value will be NULL and will result in an error.
Is there anything that they should implement ?
How can they call a function periodically?