This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: How to disable GPU DVFS & pvrsrvkm.ko error

Part Number: TDA4VM

Hi,

There are several pvrsrvkm.ko runtime errors occurred during GPU testing. 
I found that the frequency of GPU is different, it‘s 600 MHz or 750 MHz. Check that the PVR_DVFS macro in the driver source code is not open.
I want to know the reason for this,  and how to disable GPU DVFS.
[06:40:40:137][61078.530958] PVR_K:  236: RGX FW State: NOT RESPONDING - KCCB stalled (HWRState 0x00000001: HWR OK; )
[06:40:40:152][61078.542465] PVR_K:  236: RGX FW Power State: RGXFWIF_POW_IDLE (APM disabled: 0 ok, 0 denied, 0 non-idle, 0 other, 0 total. Latency: 100 ms)
[06:40:40:168][61078.558306] PVR_K:  236: RGX DVFS: 0 frequency changes. Current frequency: 600 MHz (sampled at 378ce2cd2c6e)
[06:40:40:168][61078.574125] PVR_K:  236: RGX FW OS 0 State: 0x00000003 (Active: Yes, Freelists: Ok, Grow Request Pending: No)
[06:40:40:168][61078.586609] PVR_K:  236: RGX FW OS 1 State: 0x00000002 (Active: No, Freelists: Ok, Grow Request Pending: No)
[  325.086193] PVR_K:  182: RGX FW State: NOT RESPONDING - KCCB stalled (HWRState 0x00000001: HWR OK; )
[  325.086197] PVR_K:  182: RGX FW Power State: RGXFWIF_POW_IDLE (APM disabled: 0 ok, 0 denied, 0 non-idle, 0 other, 0 total. Latency: 100 ms)
[  325.086202] PVR_K:  182: RGX DVFS: 0 frequency changes. Current frequency: 750 MHz (sampled at 4bb084cdb6)
[  325.086204] PVR_K:  182: RGX FW OS 0 State: 0x00000003 (Active: Yes, Freelists: Ok, Grow Request Pending: No)
[  325.086207] PVR_K:  182: RGX FW OS 1 State: 0x00000002 (Active: No, Freelists: Ok, Grow Request Pending: No)
SDK version: PROCESSOR-SDK-LINUX-J721E_07.02.00.07
pvrsrvkm.ko MD5: fde193aebf55879625be2cf3caa5b8c0
Thanks,
Chen Zongsheng