vx_app_signle_cam. out is failing because it is looking for img_test.rw which is not provided in the test data in RTOS downloads
Camera is connected in port 4 of the Fusion board and the initialization is fine
Please find the below logs
root@j7-evm:/opt/vision_apps# ./vx_app_single_cam.out
APP: Init ... !!!
MEM: Init ... !!!
MEM: Initialized DMA HEAP (fd=4) !!!
MEM: Init ... Done !!!
IPC: Init ... !!!
IPC: Init ... Done !!!
REMOTE_SERVICE: Init ... !!!
REMOTE_SERVICE: Init ... Done !!!
104.315179 s: GTC Frequency = 200 MHz
APP: Init ... Done !!!
104.317257 s: VX_ZONE_INIT:Enabled
104.317279 s: VX_ZONE_ERROR:Enabled
104.317285 s: VX_ZONE_WARNING:Enabled
104.319829 s: VX_ZONE_INIT:[tivxInit:71] Initialization Done !!!
104.320023 s: VX_ZONE_INIT:[tivxHostInit:48] Initialization Done for HOST !!
Single Camera Demo - (c) Texas Instruments 2019
========================================================
Usage,
./vx_app_single_cam.out --cfg <config file>
Defaulting to interactive mode
IttCtrl_registerHandler: command echo registered at location 0
IttCtrl_registerHandler: command iss_read_2a_params registered at location 1
IttCtrl_registerHandler: command iss_write_2a_params registered at location 2
IttCtrl_registerHandler: command iss_raw_save registered at location 3
IttCtrl_registerHandler: command iss_yuv_save registered at location 4
IttCtrl_registerHandler: command iss_read_sensor_reg registered at location 5
IttCtrl_registerHandler: command iss_write_sensor_reg registered at location 6
IttCtrl_registerHandler: command dev_ctrl registered at location 7
IttCtrl_registerHandler: command iss_send_dcc_file registered at location 8
NETWORK: Opened at IP Addr = 0.0.0.0, socket port=5000!!!
104.321783 s: ISS: Enumerating sensors ... !!!
104.721504 s: ISS: Enumerating sensors ... found 0 : IMX390-UB953_D3
104.721546 s: ISS: Enumerating sensors ... found 1 : AR0233-UB953_MARS
104.721551 s: ISS: Enumerating sensors ... found 2 : AR0820-UB953_LI
104.721557 s: ISS: Enumerating sensors ... found 3 : UB9xxx_RAW12_TESTPATTERN
104.721562 s: ISS: Enumerating sensors ... found 4 : UB96x_UYVY_TESTPATTERN
104.721567 s: ISS: Enumerating sensors ... found 5 : GW_AR0233_UYVY
Select camera port index 0-7 : 4
0x6 registered sensor drivers
a : IMX390-UB953_D3
b : AR0233-UB953_MARS
c : AR0820-UB953_LI
d : UB9xxx_RAW12_TESTPATTERN
e : UB96x_UYVY_TESTPATTERN
f : GW_AR0233_UYVY
Select a sensor above or press '0' to autodetect the sensor : Invalid selection
. Try again
0x6 registered sensor drivers
a : IMX390-UB953_D3
b : AR0233-UB953_MARS
c : AR0820-UB953_LI
d : UB9xxx_RAW12_TESTPATTERN
e : UB96x_UYVY_TESTPATTERN
f : GW_AR0233_UYVY
Select a sensor above or press '0' to autodetect the sensor : b
Sensor selected : AR0233-UB953_MARS
LDC Selection Yes(1)/No(0) : LDC Selection Yes(1)/No(0) : 1
Querying AR0233-UB953_MARS
113.037830 s: ISS: Querying sensor [AR0233-UB953_MARS] ... !!!
113.037968 s: ISS: Querying sensor [AR0233-UB953_MARS] ... Done !!!
113.037976 s: ISS: Initializing sensor [AR0233-UB953_MARS], doing IM_SENSOR_!
113.038055 s: ISS: Initializing sensor [AR0233-UB953_MARS], doing IM_SENSOR_!
115.636248 s: ISS: Initializing sensor [AR0233-UB953_MARS] ... Done !!!
read_test_image_raw : Unable to open file /opt/vision_apps/test_data/img_test.rw
app_create_viss : sensor_dcc_id = 233
Enabling LDC
Creating LDC
Scaler is enabled
==========================
Demo : Single Camera w/ 2A
==========================
p: Print performance statistics
s: Save Sensor RAW, VISS Output and H3A output images to File System
e: Export performance statistics
u: Update DCC from File System
x: Exit
Enter Choice:
Unsupported command
==========================
Demo : Single Camera w/ 2A
==========================
p: Print performance statistics
s: Save Sensor RAW, VISS Output and H3A output images to File System
e: Export performance statistics
u: Update DCC from File System
x: Exit
Enter Choice: 115.689113 s: ISS: Starting sensor [AR0233-UB953_MARS] ... !!!
116.227333 s: ISS: Starting sensor [AR0233-UB953_MARS] ... !!!
get_dcc_dir_size : Could not open directory or directory is empty /opt/vision_a
[ 129.742470] Initializing XFRM netlink socket
[ 132.522359] process 'docker/tmp/qemu-check041114531/check' started with execk