Other Parts Discussed in Thread: OMAP-L137
I tried to test the OMAP-L137 DSPLINK example refer “http://processors.wiki.ti.com/index.php/Example_application_using_DSP_Link_on_OMAPL1x”, but but not work out, the process as below.
Do you have any suggestion about this issue? Thank you very much!
Linux Kernel is montavista linux-2.6.18_pro500,file system is ramdisk.gz get from “/opt/mv_pro_5.0/montavista/pro/devkit/arm/v5t_le/images/ramdisk.gz” of
# mount -t nfs -o nolock 192.168.0.127:/home/fish/workdir/filesys /mnt
# cd /mnt/dsplink_test/hellodsp/module/
# ./loadmodules.sh
dsplinkk: no version for "struct_module" found: kernel tainted.
DSPLINK Module (1.61.03) created on Date: Apr 16 2009 Time: 18:37:23
# lsmod
Module Size Used by Tainted: GF
dsplinkk 188260 0 - Live 0xbf000000
# rm -f /dev/dsplink
# mknod /dev/dsplink c 230 0
# ./helloDSPgpp helloDSP.out 2
./helloDSPgpp: error while loading shared libraries: libpthread.so.0: cannot open shared object file: No such file or directory
# cd lib/
# ls
ld-2.5.90.so libm.so.6 libresolv-2.5.90.so
ld-linux.so.3 libnsl-2.5.90.so libresolv.so.2
libblkid.so.1 libnsl.so.1 libthread_db-1.0.so
libblkid.so.1.0 libnss_dns-2.5.90.so libthread_db.so.1
libc-2.5.90.so libnss_dns.so.2 libutil-2.5.90.so
libc.so.6 libnss_files-2.5.90.so libutil.so.1
libcrypt-2.5.90.so libnss_files.so.2 libuuid.so.1
libcrypt.so.1 libpam.so.0 libuuid.so.1.2
libdl-2.5.90.so libpam.so.0.79 libwrap.so.0
libdl.so.2 libpam_misc.so.0 libwrap.so.0.7.6
libgcc_s.so libpam_misc.so.0.79 lsb
libgcc_s.so.1 libpamc.so.0 security
libm-2.5.90.so libpamc.so.0.79
#