Part Number: AM6442
Hi ,
We have a board with am6442 chip with dual mac running processor sdk 8.0 device tree file.
We can see both the eth0 and eth1 ethernet while running the ifconfig command .
eth0 is getting the ip address and working fine but eth1 is not gettiing the ip address.
When we try to activate the network with 'ifup' command ,it is showing the error below.We have added the pinmuxing in the
device tree file.
***************************************************************************************
ERROR
root@am64xx-evm:~# ifup eth1 up
[ 100.291674] am65-cpsw-nuss 8000000.ethernet: phy /mdio-mux-1/mdio@1/ethernet-phy@3 not found on slave 2
ifconfig: SIOCSIFFLAGS: No such device
*******************************************************************************************
Could anyone please suggest any method or steps to solve this issue.
Any help is appreciated.
Thanks and Regards,
Radhika