Part Number: AM6442
Other Parts Discussed in Thread: TDA4VM
If you are interested in learning more about the new AM6442 Sitara Processor family and the ability to run multiple Industrial Protocols, this is a great opportunity. This is the next webinar in our monthly webinar series. There are two sessions for your convenience: One at 10AM CST for the Western Hemisphere on 10/19/2021 and another at 9PM CST (10 AM GMT + 8) for the Eastern Hemisphere 10/21/2021 (10/22/2021 in Asia). There are registration links for both sessions below.
In this webinar, we’ll step through using Codesys Control as the PLC controller to control device running EtherNet/IP adapter, PROFINET device and EtherCAT device or stacks from TI. The control and adapter/device stacks can be run on the same hardware, demonstrating the powerful flexibility of the AM64x/AM243x devices with Ethernet and ICSS-G.

Here are some things you will learn more about:
- Install and run standard Codesys Controller arm64 on AM64x Linux RT
- Connect to the Codesys development system to this runtime
- Start the TI EtherNet/IP adapter stack on AM243x and connect to Codesys
- Start and connect to PROFINET device and EtherCAT device as well
Click on your desired time slot below to register now for the event:
Session 1 - 10AM CST 10/19/2021 - Western Hemisphere
Session 2 - 9PM CST 10/21/2021 (10AM GMT+8 10/22/2021) - Eastern Hemisphere
We plan to run this webinar series on a Tuesday and Thursday (Wednesday or Friday for Asia) throughout the year.
Please visit this link to see our planned webinars, and view recording from all past webinars.
If you can't attend, a video link and the presentation material will be provided here shortly after the event. Subscribe to the post to get updates.
Also, please feel free to submit requests by replying below. We will consider all requests for topics that apply to TI Processors from Jacinto and Sitara.