Configuration:
CCS 4.2.2, recent install, includes bios 5.41.10.36, and bios 5.41.10.36
NDK 2.20.03.24
NSP 1.00.00.09
XDS100v2 from Spectrum Digital
C6748 SOM and EVM kit from Logic PD
Where are the API's for working with C6748 SOM peripherals in BIOS6?
There are no peripheral API's that show up in the help.
Do i need to add another package? How do i do that? What documents do i need to read?