Part Number: TMS320C6457
Dear sirs,
i have the necessity of use of VCP2 on DSP C64x.
In particular my code program the parameters for the VCP2 and after VCP2 Start i receive the VCPREVT on edma interrupt. (only one).
Checking the decision data respect to the input data, it work fine with input frame len <=2048.
For frame len > 2048 we receive only one VCPREVT but VCP2 remain in Running.
In all previous test, we dont have see the XEVT event!!!!
The starting code for our tests is HiBerCalculation (Texas Instrument).
Have you some indications to program the VCP2 and EDMA3 for Frame Len > 2048?
Which action the DSP code shall do when FL > 2048 fo VCP2 completion?
Thanks in advance.
Fabio