Hi,
I would like to know the list of examples available for C6657 and like to generate them.
In the processor SDK, the steps to create CCS PDK examples for C6657 are more generic for the series of processors.
Please provide the steps.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I would like to know the list of examples available for C6657 and like to generate them.
In the processor SDK, the steps to create CCS PDK examples for C6657 are more generic for the series of processors.
Please provide the steps.
How to generate the CCS PDK examples for C6657?
Pre-requisite
Steps to generate the PDK examples.
Once the processor_sdk_rtos_c665x_6_03_00_106 is installed, observe the PDK package, "pdk_c665x_2_0_16" under C:\ti

6. The following is the list of example projects which will get created. - 48 examples
| cppi_evmc6657_c66BiosExampleProject |
| cppi_evmc6657_C66BiosTestProject |
| EMAC_evmc6657_C66Loopback_testProject |
| GPIO_LedBlink_C6657_EVM_c66xTestProject |
| hyplnk_evmc6657_C66BiosExampleProject |
| hyplnk_evmc6657_C66DevLibBiosExampleProject |
| I2C_BasicExample_C6657_Evm_c66xExampleProject |
| I2C_BasicExample_C6657_Evm_c66xTestProject |
| MCBSP_evmc6657_C66DigLpbkExampleProject |
| NIMU_emacExampleClient_EVMC6657C66BiosExampleProject |
| NIMU_emacExample_EVMC6657C66BiosExampleProject |
| PCIE_evmc6657_wSoCFile_C66BiosExampleProject |
| PCIE_evmc6657_wSoCLib_C66BiosExampleProject |
| qmAcc_evmc6657_C66BiosTestProject |
| qmDCfg_evmc6657_C66BiosTestProject |
| qmDesc_evmc6657_C66BiosTestProject |
| qmInfraMC_evmc6657_C66BiosExampleProject |
| qmInfra_evmc6657_C66BiosExampleProject |
| qmInsRegion_evmc6657_C66BiosTestProject |
| qmQAlloc_evmc6657_C66BiosTestProject |
| qmQosFwCModel_evmc6657_C66BiosTestProject |
| qmQosSchedCModel_evmc6657_C66BiosTestProject |
| qmQosSchedDropSched_evmc6657_C66BiosTestProject |
| qmQosSchedWide_evmc6657_C66BiosTestProject |
| qmQosSched_evmc6657_C66BiosTestProject |
| qmQosTest_evmc6657_C66BiosTestProject |
| qmSCfg_evmc6657_C66BiosTestProject |
| qmSrioContext_evmc6657_C66BiosTestProject |
| qmSrioRtr_evmc6657_C66BiosTestProject |
| rmShared_evmc6657_C66BiosTestProject |
| rm_evmc6657_C66BiosTestProject |
| rm_evmc6657_C66DspMtBiosTestProject |
| SPI_BasicExample_C6657_c66xExampleProject |
| SPI_BasicExample_C6657_c66xTestProject |
| SRIO_Loopback_evmc6657_C66BiosTestProject |
| SRIO_LpbkDioIsr_evmc6657_C66BiosExampleProject |
| SRIO_MulticoreLpbk_evmc6657_C66BiosExampleProject |
| SRIO_TputBenchmarking_evmc6657_C66TestProject |
| tcp3d_evmc6657_C66BiosExampleProject |
| tcp3d_evmc6657_C66BiosTestProject |
| transportQmssBenchmarkC6657C66ExampleProject |
| transportSrioBenchmarkC6657C66ExampleProject |
| transportSrioMultiBoardConsumerC6657C66ExampleProject |
| transportSrioMultiBoardProducerC6657C66ExampleProject |
| UART_BasicExample_C6657_c66xDMATestProject |
| UART_BasicExample_C6657_c66xExampleProject |
| UART_BasicExample_C6657_c66xTestProject |