Other Parts Discussed in Thread: OMAPL138
Hi,
We have designed OMAPL138 based custom product. We need to use USB1.1 OHCI driver, since USB2.0 is used for other application.
We are using linux kernel from DaVinci-PSP-SDK-03.20.00.12, core is running at 372 MHz.
We are facing performance issue with USB1.1 OHCI.
Can someone give me exact performance figure for USB 1.1 OHCI driver ?
We'll be transferring data in small chunks and will use USB1.1 for data xfer.
Is there a way to tune the performance of USB 1.1? Is there any scope of improvement in performance ?
Thanks in advance,
Sweta