Other Parts Discussed in Thread: DRA722, PCF8575, PMP, TDA2EG-17
Dear all,
This is my log , What is this problem and how can I solve it?
And I use sd card to boot
====================================
CPU : DRA722-GP ES2.1
Model: TI DRA722
Board: DRA72x EVM REV
DRAM: 2 GiB
MMC: i2c_write: error waiting for data ACK (status=0x116)
pcf8575_i2c_write_le16 i2c write failed to addr 21
OMAP SD/MMC: 0, OMAP SD/MMC: 1
** First descriptor is NOT a primary desc on 1:1 **
Warning: fastboot.board_rev: unknown board revision
GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
part_get_info_efi: *** ERROR: Invalid GPT ***
GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
part_get_info_efi: *** ERROR: Invalid Backup GPT ***
ERROR: cannot find partition: 'userdata'
at arch/arm/cpu/armv7/omap-common/utils.c:199/mmc_get_part_size()
Warning: fastboot.userdata_size: unable to calc
SCSI: SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Found 0 device(s).
Hit any key to stop autoboot: 2 1 0
## Error: "update_to_fit" not defined
## Error: "findfdt" not defined
## Error: "envboot" not defined
## Error: "mmcboot" not defined
## Error: "emmc_android_boot" not defined
=======================================
Thanks!!