Other Parts Discussed in Thread: SYSBIOS
Hi,
I’ve received a question from the customer regarding PCIe connection to PC. The PCIe connection doesn’t work correctly on their own board with AM5706, so they’re now looking into this.
They’re trying to connect their own board (PCIe board) using AM5706 to a Windows PC, but it is not recognized by the device manager on the PC. Even “?” is not shown on the device manager. If the AM572x IDK is used as Root Complex, their board can be linked up with the AM572x IDK.
Do you have a sample project of AM5706 that has a track record of PCIE connection to general-purpose PCs ? If you have, could you share it with them ?
During it cannot be connected, the status of LTSSM is 0x3 (Polling.compliance).
Do you have any experience of connecting error with Polling.Compliance ? and do you have any idea to solve this ?
It would be helpful if you could share any information with them regarding not only AM57xx.
They're now using Processor SDK RTOS 7.3.
Regards, Hideaki