Part Number: PROCESSOR-SDK-J7200
I use C:/ti-processor-sdk-rtos-j7200-evm-07_03_00_07/ti-cgt-arm_20.2.0.LTS/bin/armcl.exe to complier a C file ,
This c file include a stdint.h
The stdint.h is in C:/ti-processor-sdk-rtos-j7200-evm-07_03_00_07/ti-cgt-arm_20.2.0.LTS/include
In line 6 , it code as #include <stdint.h>
I use the follow command but failed,
C:/ti-processor-sdk-rtos-j7200-evm-07_03_00_07/ti-cgt-arm_20.2.0.LTS/bin/armcl.exe -ms -c -mv7R5 --float_support=vfpv3d16 --abi=eabi --endian=little -o3 -k -g --display_error_number --diag_warning=225 --code_state=32 --fp_mode=strict -eo.o -ec.c --symdebug:dwarf --embed_inline_assembly -D_DEBUG_=1 -DBUILD_MCU2_1 -DBUILD_MCU -DAUTOSAR_421 -DSOC_J7200 -IBsw/Os/Implementation -Ilib\ti\PDK\include\ -I_gen/headers -ppa -ppd=_gen/depends/SchM_Dio.mak -fc bsw/mcal/bsw_stubs/rte/src/SchM_Dio.c -fs=_gen/objects -fr=_gen/objects
"lib\ti\PDK\include\ti/osal/HwiP.h", line 65: fatal error #1965: cannot open source file
"stdint.h"
1 catastrophic error detected in the compilation of "Bsw/Mcal/Bsw_Stubs/Rte/src/SchM_Dio.c".
Compilation terminated.
If I add a optional -IC:/ti-processor-sdk-rtos-j7200-evm-07_03_00_07/ti-cgt-arm_20.2.0.LTS/include ,
Then compiler is successfully.
But this is a bad idea, if the compliers location is changed , the command should be change,
As far as I know , If the code use #include <…> , the complier search the system include path first,
Is there any special about this complier ?
What is the system include path for this compiler ?
How can I complier this c file successfully without add the system include file ?