This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

High-bandwidth ISO mode webcam with DM365

Dear All:

 

I realize that the MUSB USB host controller of DM365 can not handle

high-bandwidth ISO mode webcam.

However, it is very difficult to find a ISO mode webcam chip which

have the packet size smaller than 1024 bytes in VGA/D1 or 720p resolution.

 

Is there any possibility to modify the linux USB or UVC driver (software workaround)

so that DM365 can use these webcam chips with high-bandwidth ISO mode?

Anyway suggestion will be welcome!

 

Best regards,

 

Ray