Part Number: TMDXIDK5718
Dear Team,
Connect the EVM Board and debug it. The following error occurred. Please lend your support in this regard.
Error
CortexA15_0: Trouble Writing Memory Block at 0x58880800 on Page 0 of Length 0x4: (Error -1141 @ 0x3D58) Device is not responding to the request. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 8.4.0.00006)
CortexA15_0: GEL: Error while executing OnTargetConnect(): Target failed to write 0x58880800
at *((unsigned int *) regAddr)=(unsigned int) 0x40000000 [AM571x_multicore_reset.gel:12]
at IPUSSClkEnable(1) [AM571x_multicore_reset.gel:236]
at IPU1SSClkEnable_API() [AM571x_multicore_reset.gel:210]
at AM571x_MULTICORE_EnableAllCores() [AM571x_startup_common.gel:42]
at OnTargetConnect()