Hi,
error compiling arm UBL 03.20.00.14 for AM1808, error messages in spiboot.c spi.c spi_mem.c like :
Symbol 'SPI_MEMORYMAP_SPACING' could not be resolved
Symbol 'Uint32' could not be resolved
Uint32 type could not be resolved
Uint16 type could not be resolved
Uint8 type could not be resolved
but .out could be generated normally.
I'm using ccsv5 to import ccsv4 projects, is that the reason problem comes? how to solve the problem?
at the end of make,
armubl-03.20.00.14/ccsv4/omapl1x8\ubl-spi.out
gmake[1]: /usr/local/CCSv5/ccsv5/tools/compiler/tms470binhex470.exe: Command not found
gmake[1]: [post-build] Error 127 (ignored)
regards,
Pan