Part Number: PROCESSOR-SDK-AM64X
Other Parts Discussed in Thread: SYSCONFIG
Hello,
I am using the SDK 08.00.00.
I want to trigger a reset to the AM64 which shall cause it to issue a reboot and start with the Bootloader again.
Some research brought me to the DMSC-Module and the SCI-function Sciclient_pmDeviceReset. As I think will be the right option, but I'm not sure. Can I call this function from every of the R5F-Cores without problems and do I need to do some additional configuration steps in SysConfig?
And are their more possibilities of the reset behaviour of the SoC and if so are they documented somewhere?
Best regards
Felix