Part Number: TMS320C6652
Hi Shankari,
I don't want to build the DSPLIB, I just want to include the DSPF_sp_ifftSPxSP.sa into my project.
here's my main():
/**
* main.c
*/
#include <c6x.h>
#include "DSPF_sp_ifftSPxSP.h"
#define FFT_LEN 8192 // complex values
#define FFT_RAD 4
float IFFT_Twid[2*FFT_LEN];
float InpBuf [2*FFT_LEN];
float OutBuf [2*FFT_LEN];
unsigned char brev[64];
int main(void)
{
DSPF_sp_ifftSPxSP (FFT_LEN, OutBuf, IFFT_Twid, InpBuf, brev, FFT_RAD, 0, FFT_LEN); // cyc=?/FFT_L=8k; DSPLIB src 3_4_0_0
return 0;
}
I included DSPF_sp_ifftSPxSP.sa by -> Add Files...
CCS does not build the project (error see above).
BR Gerold