This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C5515



Hello,

Is it mandatory to connect VBUS of the USB connector to the USB_VBUS pin of the USB port of DSP Or it's sufficient to connect USB_VBUS pin of DSP to the internal on board voltage constantly? 2. Can USB_VBUS pin of the DSP be connected to 3.3V instead of 5V voltage? Thanks in advance

Best Regards

Yaron 

  • 1. If you plan to use USB interface in your system; then yes, the USB_VBUS pin must be connected to the USB interface's VBUS. This will be used to detect the USB connection.

    2. If you don't plan to use USB interface in your system, then the USB_VBUS pin must be connected to ground.

     

    Regards

    Wen

  • We are using the USB but since we use a galvanic isolator the voltage drop to 3.3V, can the DSP USB VBUS can detect 3.3V? Thanks, Yaron
  • I am not sure if the USB connection will be reliably detected via the isolator. The USB PHY interface of C55515/5505 will follow the USB 2.0 standard, so if there is any violation cause by the isolator, then there will be a problem.

    Thanks and regards

    Wen

  •  

    Hello Wen,

    USB isolator that we use is a special USB isolator that is intended to work with USB 2.0. Let me clarify my question, is it enough to set 3.3V on Vbus that the C5515 will recognize USB connection or only 5V must be connected to Vbus. About isolator. I used this isolator chip for USB isolation with PIC32F795 of Microchip and it works properly.

    Thanks,

    Yaron