This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: Time Sync Router: available timers for HW Push

Part Number: TDA4VM

Hi Team,

In the training material provided with the SDK ("docs/trainings/TimeSync_design_overview.pdf"), reference is made to using "DM TIMER[14-19] / GTC0" as the triggers for hardware push events from the CPTS for multi-core sync.

I can't seem to find anything in the reference manual showing that only timers 14-19 can be used for this purpose.

So my question is, can only these 6 timers be used in the main domain?  If so, why, and where can I find relevant information about this?
And similarly for the MCU domain, can any of the 10 MCU timers be used, or only some?

Thanks very much,

-JP