This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: with ethfw How to change the TDA4 A72 network segment ?

Part Number: TDA4VM

hi expert:

  with SDK_08 , I comile the ethfw with disable DHCP  ( #define ETHAPP_LWIP_USE_DHCP  (0)), with this marco .  the ethfw (server )will have a static  host IP (192.168.1.200) , and , after the Linux run on A72 , which will load the ethfw on mcu2_0 , the eth0 , eth1  will have a 192.168.1.* network segement IP .

 I just want to know , who allocate the IP to eth0 /eth1 ,  our ethfw ? and how I can change the network segment ?

  • Hi,

    You can use ifconfig <eth interface> <ip address> command to set IP address and other parameters, the Linux virtual driver communicates with Ethernet FW to set the ARP table

    Regards

    Vineet

  • hi Vineet:

     Yes , I know youe method to change the Linux eth ipaddr , but I want to know if the IPs are allocated by ethfw ? and if the IP are allocated by ethfw , how Can I update the DHCP allocate network segment?