Part Number: TMS320C6678
Hello,
I am dealing with a peculiar linker error message.
The project I am working with has a linkInfo.xml file which is throwing a fatal error #6001: cannot open file: Invalid argument.
I have not seen this error before and I would like clarification as to what it means.
The linkInfo.xml file exists in the main project directory. Permissions are set to full control for all users.
I have performed a clean on the project and even restarted CCS.
I am using Windows 10 and CCS 10.2
The exact error is below:
<Linking>
fatal error #6001: cannot open file "Core0_linkInfo.xml": Invalid argument
This project has been compiling all along until now.
I changed one library, the IPC library, which I rebuilt according to the instructions in the users guide.
The rebuilt library was rebuilt using the same version of the compiler 8.3.3 as the rest of the project.
Please Advise,
Forrest