Part Number: 66AK2E05
Hello,
we try to use the mcp2515 (CAN BUS to SPI) chip with no success.
It is connected on the spi1 bus of our ARM processor (KEYSTONE II - 66AK2E05), the interrupt PIN of the chip is connected on the GPIO-5 pin of the CPU too.
We are developing our Software (OS + Apps) using the:
TI ΚΕΥΣΤΟΝΕ ΙΙ - SDK
v06.03.00.106
Linux kernel src:
linux-4.19.94+gitAUTOINC+be5389fd85-gbe5389fd85
I order to enable the specific CAN driver, the following lines has been added to the linux kernel configuration
CONFIG_CAN=y
CONFIG_CAN_MCP251X=m
Also, the following lines has been added ( according to <kernel documentation > ) to our custom board device tree, which is based on keystone-k2e-evm.dts file.
&spi1 {
....
can0: mcp2515@0 {
compatible = "microchip,mcp2515";
reg = <0>;
spi-max-frequency = <1000000>;
clocks = <&canclk>;
interrupt-parent = <&gpio0>;
interrupts = <5 IRQ_TYPE_EDGE_FALLING>;
}
....
}
&soc0 {
...
canclk: canclk {
compatible = "fixed-clock";
#clock-cells = <0>;
clock-frequency = <8000000>;
clock-output-names = "can-clk";
};
...
}
When building the DTB we get the warning below:
Warning (interrupts_property): /soc@0/gpio@260bf00: Missing interrupt-controller or interrupt-map property
Warning (interrupts_property): /soc@0/gpio@260bf00: Missing #interrupt-cells in interrupt-parent
After booting the system, the `dmesg` command shows
root@ccm:~# dmesg | grep mcp
[ 11.995130] mcp251x spi1.0 can0: MCP2515 successfully initialized.
Then, we setup our CAN controller with:
ip link set can0 type can bitrate 250000
ip link set up can0
At this point we have to situations:
1) If we do not patch the linux kernel mcp2515 driver
Then, the mcp2515 driver tries to acquire IRQ, but it gets a `0` assigned and it fails.
PS: We also tried adding interrupt-controller and #interrupt-cells properties in gpio0 in DTB but it did not help.
2) If we do patch the linux kernel mcp2515 driver
If we hard code the IRQ assignment (which is not obviously a solution) by adding
mcp251x.c, line ~943, function `static int mcp251x_open(struct net_device *net)` :
int oldIrq = spi->irq;
spi->irq=gpio_to_irq(5);
printk("mcp251x spi->irq: set from %i to %i (IRQ on GPIO-5 PIN)\n",oldIrq,spi->irq);
in the mcp251x.c src file, then the device is showing up as can0 and the `ifconfig can0` command shows:
can0 Link encap:UNSPEC HWaddr 00-00-00-00-00-00-00-00-00-00-00-00-00-00-00-00
UP RUNNING NOARP MTU:16 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:10
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B
Also the `dmesg` command shows
root@ccm:~# dmesg | grep mcp
[ 11.995130] mcp251x spi1.0 can0: MCP2515 successfully initialized.
...
[ 1758.176391] mcp251x spi->irq: set from 0 to 41 (IRQ on GPIO-5 PIN)
...
Then, from a windows PC, we use a USB to CAN controller in order to send / receive CAN data .
The wire CAN connection between the 2 controllers is checked and it is correct!
By sending data from windows PC to our Linux KEYSTONE II board, the windows CAN controller reports no transmission errors and by running `candump can0` command at the linux side we should see something like:
<< can0 001 [8] 11 22 33 44 55 66 77 88 >>
but we get nothing.
No data are received by the Linux KEYSTONE II board.
Also if we try to send data from the Linux KEYSTONE II board with the `cansend can0 001#1122334455667788` command,
then on the windows PC, using the CAN to USB controller software we see that no data are received too...
In any of the mentioned steps (Loading linux kernel, loading the CAN driver, attempt of sending/receiving data) the linux kernel does not produce any IRQ....
The `cat /proc/interrupts` command shows that at IRQ 41 (hard coded GPIO-5 <-> IRQ in CAN driver the counter value is always `0`
CPU0 CPU1 CPU2 CPU3
17: 0 0 0 0 GICv2 29 Level arch_timer
18: 619776 613791 609211 618116 GICv2 30 Level arch_timer
21: 0 0 0 0 GICv2 142 Edge timer-keystone
22: 0 0 0 0 GICv2 52 Edge arm-pmu
23: 0 0 0 0 GICv2 53 Edge arm-pmu
24: 0 0 0 0 GICv2 54 Edge arm-pmu
25: 0 0 0 0 GICv2 55 Edge arm-pmu
26: 1 0 0 0 GICv2 36 Edge 26202a0.keystone_irq
27: 9038 0 0 0 GICv2 309 Edge ttyS0
28: 241675 0 0 0 GICv2 312 Edge
29: 8 0 0 0 GICv2 315 Edge 2530000.i2c
30: 0 0 0 0 GICv2 318 Edge 2530400.i2c
31: 0 0 0 0 GICv2 321 Edge 2530800.i2c
32: 110 0 0 0 GICv2 324 Edge 21000400.spi
33: 39 0 0 0 GICv2 328 Edge 21000600.spi
34: 2 0 0 0 GICv2 332 Edge 21000800.spi
35: 0 0 0 0 GICv2 184 Edge 2680000.usb, xhci-hcd:usb1
41: 0 0 0 0 GPIO-AINTC 157 Edge mcp251x
68: 0 0 0 0 GICv2 70 Edge ks-pcie-error-irq
70: 0 0 0 0 GICv2 446 Edge 25000000.usb, xhci-hcd:usb3
71: 0 0 0 0 GICv2 417 Edge ks-pcie-error-irq
80: 0 0 0 0 PCI-MSI 0 Edge PCIe PME, aerdrv
89: 0 0 0 0 PCI-MSI 134217728 Edge PCIe PME, aerdrv
98: 0 0 0 0 GICv2 80 Level hwqueue-528
99: 7882 0 0 0 GICv2 81 Level hwqueue-529
100: 5221 0 0 0 GICv2 82 Level hwqueue-530
101: 0 0 0 0 GICv2 83 Level hwqueue-531
102: 0 0 0 0 GICv2 84 Level hwqueue-532
103: 7859 0 0 0 GICv2 85 Level hwqueue-533
104: 6739 0 0 0 GICv2 86 Level hwqueue-534
105: 0 0 0 0 GICv2 87 Level hwqueue-535
130: 1 0 0 0 keystone-irq 0 Edge 10800000.dsp
131: 0 0 0 0 keystone-irq 8 Edge dsp0
IPI0: 0 0 0 0 CPU wakeup interrupts
IPI1: 0 0 0 0 Timer broadcast interrupts
IPI2: 252323 228722 241768 263646 Rescheduling interrupts
IPI3: 3 7 10 8 Function call interrupts
IPI4: 0 0 0 0 CPU stop interrupts
IPI5: 3 0 1 481 IRQ work interrupts
IPI6: 0 0 0 0 completion interrupts
Err: 0
Debugging info:
With help of an oscilloscope, we observer:
While loading the linux kernel and after loading the mcp251x driver, the GPIO-5 pin value is HIGH (1)
and we also see on the SPI BUS that `some` data are exchanged between the linux kernel and the chip.
After setting up the chip with the following commands,
ip link set can0 type can bitrate 250000
ip link set up can0
we see that the GPIO-5 pin value is changing to LOW (0)
From that point the CAN communication between the windows PC and the Linux board with the mcp251x chip is not responding (no transmission/reception of any data)...
It seems that the Keystone/davinci GPIO driver is not working properly.
Any suggestions/ideas on how we can solve this problem would be appreciated.
Regards,
Ioannis.