Part Number: AM5718
Hi, we are driving DE mode LCD. In Linux, we see below configuration need to set. It seems that these parameters are for hysnc/vsync mode LCD. Our question is where to set for DE LCD? If there is no other place to set, how to convert the LCD's DE timing requirment to hysnc/vsync? Is it hfront-porch + hback-porch +hsync-len = DE inactive duration? The LCD DE timing spec also attached below.
display-timing bindings
=======================
display-timings node
--------------------
required properties:
- none
optional properties:
- native-mode: The native mode for the display, in case multiple modes are
provided. When omitted, assume the first node is the native.
timing subnode
--------------
required properties:
- hactive, vactive: display resolution
- hfront-porch, hback-porch, hsync-len: horizontal display timing parameters
in pixels
vfront-porch, vback-porch, vsync-len: vertical display timing parameters in
lines
- clock-frequency: display clock in Hz
optional properties:
- hsync-active: hsync pulse is active low/high/ignored
- vsync-active: vsync pulse is active low/high/ignored
- de-active: data-enable pulse is active low/high/ignored
- pixelclk-active: with
- active high = drive pixel data on rising edge/
sample data on falling edge
- active low = drive pixel data on falling edge/
sample data on rising edge
- ignored = ignored
- syncclk-active: with
- active high = drive sync on rising edge/
sample sync on falling edge of pixel
clock
- active low = drive sync on falling edge/
sample sync on rising edge of pixel
clock
- omitted = same configuration as pixelclk-active
- interlaced (bool): boolean to enable interlaced mode
- doublescan (bool): boolean to enable doublescan mode
- doubleclk (bool): boolean to enable doubleclock mode
All the optional properties that are not bool follow the following logic:
<1>: high active
<0>: low active
omitted: not used on hardware
There are different ways of describing the capabilities of a display. The
devicetree representation corresponds to the one commonly found in datasheets
for displays. If a display supports multiple signal timings, the native-mode
can be specified.
The parameters are defined as:
+----------+-------------------------------------+----------+-------+
| | ^ | | |
| | |vback_porch | | |
| | v | | |
+----------#######################################----------+-------+
| # ^ # | |
| # | # | |
| hback # | # hfront | hsync |
| porch # | hactive # porch | len |
|<-------->#<-------+--------------------------->#<-------->|<----->|
| # | # | |
| # |vactive # | |
| # | # | |
| # v # | |
+----------#######################################----------+-------+
| | ^ | | |
| | |vfront_porch | | |
| | v | | |
+----------+-------------------------------------+----------+-------+
| | ^ | | |
| | |vsync_len | | |
| | v | | |
+----------+-------------------------------------+----------+-------+
Note: In addition to being used as subnode(s) of display-timings, the timing
subnode may also be used on its own. This is appropriate if only one mode
need be conveyed. In this case, the node should be named 'panel-timing'.