This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM57X: SPI Slave part code

Part Number: PROCESSOR-SDK-AM57X
Other Parts Discussed in Thread: SN65HVS882

Hi all,

I am using

BOARD : TMDXIDKAM5718

Processor SDK version :ti-processor-sdk-linux-am57xx-evm-06.03.00.106
Linux version : linux-4.19.94+gitAUTOINC+be5389fd85-gbe5389fd85
U-boot Version : u-boot-2019.01+gitAUTOINC+333c3e72d3-g333c3e72d3

In idk board spi slave device is sn65hvs882, i am working this slave. 

processor sdk according spi slave pisosr-gpio driver is present but i could able to check through this driver. for this reason i enabled spidev3.0 (dev/spidev3.0) as below 

am57xx-idk-common-dtsi file

&mcspi3 {
status = "okay";
ti,no-idle;
ti,no-reset-on-init;

spidev@3 {
compatible = "linux,spidev";
spi-max-frequency = <1000000>;
reg = <0>;
#address-cells = <1>;
#size-cells = <0>;
ti,hwmods = "mcspi3";
ti,spi-num-cs = <1>;
};
};

user space code

int spi_test()
{
int ret = 0;
int fd;

gpio_loaddata();

fd = open(device, O_RDWR);
if (fd < 0)
pabort("can't open device");

/*
* spi mode
*/
mode |= SPI_MODE_2;

ret = ioctl(fd, SPI_IOC_WR_MODE32, &mode);
if (ret == -1)
pabort("can't set spi mode");

ret = ioctl(fd, SPI_IOC_RD_MODE32, &mode);
if (ret == -1)
pabort("can't get spi mode");


/* bits per word
*/
ret = ioctl(fd, SPI_IOC_WR_BITS_PER_WORD, &bits);
if (ret == -1)
pabort("can't set bits per word");

ret = ioctl(fd, SPI_IOC_RD_BITS_PER_WORD, &bits);
if (ret == -1)
pabort("can't get bits per word");

/*
* max speed hz
*/
ret = ioctl(fd, SPI_IOC_WR_MAX_SPEED_HZ, &speed);
if (ret == -1)
pabort("can't set max speed hz");

ret = ioctl(fd, SPI_IOC_RD_MAX_SPEED_HZ, &speed);
if (ret == -1)
pabort("can't get max speed hz");

printf("spi mode: 0x%x\n", mode);
printf("bits per word: %d\n", bits);
printf("max speed: %d Hz (%d KHz)\n", speed, speed/1000);

if (input_tx && input_file)
pabort("only one of -p and --input may be selected");

if (input_tx)
transfer_escaped_string(fd, input_tx);
else if (input_file)
transfer_file(fd, input_file);
else if (transfer_size) {
struct timespec last_stat;

clock_gettime(CLOCK_MONOTONIC, &last_stat);

while (iterations-- > 0) {
struct timespec current;

transfer_buf(fd, transfer_size);

clock_gettime(CLOCK_MONOTONIC, &current);
if (current.tv_sec - last_stat.tv_sec > interval) {
show_transfer_rate();
last_stat = current;
}
}
printf("total: tx %.1fKB, rx %.1fKB\n",
_write_count/1024.0, _read_count/1024.0);
} else
transfer(fd, default_tx, default_rx,1);// sizeof(default_tx));

close(fd);

return ret;

}

//transfer function definition

static void transfer(int fd, uint8_t const *tx, uint8_t const *rx, size_t len)
{
int ret;
int out_fd;
struct spi_ioc_transfer tr = {
.tx_buf = (unsigned long)tx,
.rx_buf = (unsigned long)rx,
.len = len,
.delay_usecs = delay,
.speed_hz = speed,
.bits_per_word = bits,
};

if (mode & SPI_TX_QUAD)
tr.tx_nbits = 4;
else if (mode & SPI_TX_DUAL)
tr.tx_nbits = 2;
if (mode & SPI_RX_QUAD)
tr.rx_nbits = 4;
else if (mode & SPI_RX_DUAL)
tr.rx_nbits = 2;
if (!(mode & SPI_LOOP)) {
if (mode & (SPI_TX_QUAD | SPI_TX_DUAL))
tr.rx_buf = 0;
else if (mode & (SPI_RX_QUAD | SPI_RX_DUAL))
tr.tx_buf = 0;
}

ret = ioctl(fd, SPI_IOC_MESSAGE(1), &tr);
if (ret < 1)
pabort("can't send spi message");

if (verbose)
hex_dump(tx, len, 32, "TX");

if (output_file) {
out_fd = open(output_file, O_WRONLY | O_CREAT | O_TRUNC, 0666);
if (out_fd < 0)
pabort("could not open output file");

ret = write(out_fd, rx, len);
if (ret != len)
pabort("not all bytes written to output file");

close(out_fd);
}

if (verbose)
hex_dump(rx, len, 32, "RX");
}

i can write the data based on this code but i couldn't  able to read. (note: i made hardware connection )

could you please help me to test this spi slave in idk board .

thanks and regards

chandana