This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Does TDA4VM support CAN and PCIE drivers in QNX?
How can I use CAN or PCIE tools on QNX?
Do I need QNX or TI to provide additional BSP drivers?
Thank you!
Hi,
The TI PSDK QNX release does not include support for PCIe or CAN for QNX on the A72.
Yes, QNX can be contacted for this functionality.
In the case of CAN, the PSDK RTOS release has CAN driver code that could be also considered for porting to the A72.
ti-processor-sdk-rtos-j721e-evm-08_00_00_12//mcusw/mcal_drv/mcal/Can/
ti-processor-sdk-rtos-j721e-evm-08_00_00_12/pdk_jacinto_08_00_00_37/packages/ti/csl/src/ip/mcan
Regards,
kb