Hi to all,
while the kernel booting in beagleboard i am getting this error at the end
Loading kernel modules for gstreamer-ti...
Running /usr/share/ti/gst/omap3530/loadmodules.shFATAL: Module cmemk not found.
FATAL: Module dsplinkk not found.
FATAL: Module lpm_omap3530 not found.
FATAL: Module sdmak not found.
when try to run opencv programs while running an application it shows below error
CMEM Error: init: Failed to open /dev/cmem: 'No such file or directory'
CMEM Error: CMEM file descriptor -1 (failed 'open()'), ensure CMEMK kernel module cmemk.ko has been installed with 'insmod'OpenCV Error: Insufficient memory (Failed to5
terminate called after throwing an instance of 'cv::Exception'
what(): /home/engrprabhu/oe/angstrom-angstrom-setup-scripts/build/tmp-angstrom_2008_1/work/armv7a-angstrom-linux-gnueabi/opencv-2.2.0+svnr4812-r1/opencv/modules/corr
Aborted
what i should do... help me..
Thanks
Prabhu