This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Possible to customize the display through the DM814x M3 BIOS Firmware and use it without Syslink?

My intention is to let HDVPSS output graphic image through the LCD port (e.g., DVO). And if HDVPSS is running with the M3 Firmware as default configuration, can I output graphical data to LCD display by just writing data through the frame buffer, without using Syslink?

I am not using Linux or WinCE. And I would like to know if Syslink is able to be built with a standalone runable program.

I assume the HDVPSS can be intially configured properly and run as is without the need to change the setting? Just getting the data from the frame buffer and output to LCD?

Thanks in advance.

Philip